Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum MKR1000 not starting from LIPO
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 414 subscribers
  • Views 284 views
  • Users 0 members are here
  • wifi
  • dht22
  • mkr1000
  • dht11
Related

MKR1000 not starting from LIPO

gharryh
gharryh over 9 years ago

For some days now i am trying to build a simple system to measure temp. and hum. using a DHT22 sensor connected to a MKR100 that has a 3.7V 1000maH Li-On acuu..

 

I wrote a sketch that acts as a webserver displaying some data on a webpage. This the skektch:

 

/*
  WiFi Web Server

  A simple web server that shows the value of the analog input pins.
  using a WiFi shield.

  This example is written for a network using WPA encryption. For
  WEP or WPA, change the WiFi.begin() call accordingly.

  Circuit:
   WiFi shield attached
   Analog inputs attached to pins A0 through A5 (optional)

  created 13 July 2010
  by dlf (Metodo2 srl)
  modified 31 May 2012
  by Tom Igoe

*/

#include "DHT.h"
#define DHTPIN 6     // what digital pin we're connected to
#include <SPI.h>
#include <WiFi101.h>
#include <WiFiMDNSResponder.h>

char ssid[] = "TimeTech"; //  your network SSID (name)
char pass[] = "secret";    // your network password (use for WPA, or use as key for WEP)
//int status = WL_IDLE_STATUS;

//char ssid[] = "yourNetwork";      // your network SSID (name)
//char pass[] = "secretPassword";   // your network password
int keyIndex = 0;                 // your network key Index number (needed only for WEP)

int status = WL_IDLE_STATUS;

// Uncomment whatever type you're using!
//#define DHTTYPE DHT11   // DHT 11
#define DHTTYPE DHT22   // DHT 22  (AM2302), AM2321
//#define DHTTYPE DHT21   // DHT 21 (AM2301)

// Connect pin 1 (on the left) of the sensor to +5V
// NOTE: If using a board with 3.3V logic like an Arduino Due connect pin 1
// to 3.3V instead of 5V!
// Connect pin 2 of the sensor to whatever your DHTPIN is
// Connect pin 4 (on the right) of the sensor to GROUND
// Connect a 10K resistor from pin 2 (data) to pin 1 (power) of the sensor

// Initialize DHT sensor.
// Note that older versions of this library took an optional third parameter to
// tweak the timings for faster processors.  This parameter is no longer needed
// as the current DHT reading algorithm adjusts itself to work on faster procs.
DHT dht(DHTPIN, DHTTYPE);

float tF;
float dP;
float dPF;

int countIndex=0;

WiFiServer server(80);

void setup() {
  //Initialize serial and wait for port to open:
  Serial.begin(9600);
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }

  // check for the presence of the shield:
  if (WiFi.status() == WL_NO_SHIELD) {
    Serial.println("WiFi shield not present");
    // don't continue:
    while (true);
  }
  IPAddress ip(192, 168, 178, 222);

  WiFi.config(ip);
  
//  analogReference();

//  for(int i=0; i<8; i++; analogRead(A0));
  
  // attempt to connect to WiFi network:
  while ( status != WL_CONNECTED) {
    Serial.print("Attempting to connect to SSID: ");
    Serial.println(ssid);
    // Connect to WPA/WPA2 network. Change this line if using open or WEP network:
    status = WiFi.begin(ssid, pass);

    // wait 10 seconds for connection:
    delay(10000);
  }
  server.begin();
  // you're connected now, so print out the status:
  printWiFiStatus();
}


void loop() {
  // listen for incoming clients
  WiFiClient client = server.available();
  if (client) {
    Serial.println("new client");
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        Serial.write(c);
        // if you've gotten to the end of the line (received a newline
        // character) and the line is blank, the http request has ended,
        // so you can send a reply
        if (c == '\n' && currentLineIsBlank) {
          // send a standard http response header
          client.println("HTTP/1.1 200 OK");
          client.println("Content-Type: text/html");
          client.println("Connection: close");  // the connection will be closed after completion of the response
          client.println("Refresh: 5");  // refresh the page automatically every 5 sec
          client.println();
          client.println("<!DOCTYPE HTML>");
          client.println("<html>");

          int sensorValue1 = analogRead(A1);
          int sensorValue3 = analogRead(A3);

          float voltage1 = sensorValue1 * (3.3 / 1023.0);
          float voltage3 = sensorValue3 * (3.3 / 1023.0);

          client.print("analog input1 ");

          client.print(" is ");
          client.print(voltage1);
          client.println(" V<br />");
          client.print("analog input3 ");

          client.print(" is ");
          client.print(voltage3);
          client.println(" V<br />");
         client.println("<br />");

          // Read temperature as Celsius (the default)
          float t = dht.readTemperature();
          countIndex++;
          float h = dht.readHumidity();
          client.print("Aantal meetingen vandaag: ");
          client.println(countIndex);
          client.print("<BR />");
          client.print("Temperatuur: ");
          client.print(t);
          client.print("℃<BR />");
          client.print("Luchtvochtigheid: ");
          client.print(h);
          client.print("%<BR />");
          client.println("</html>");
          break;
        }
        if (c == '\n') {
          // you're starting a new line
          currentLineIsBlank = true;
        }
        else if (c != '\r') {
          // you've gotten a character on the current line
          currentLineIsBlank = false;
        }
      }
    }
    // give the web browser time to receive the data
    delay(1);

    // close the connection:
    client.stop();
    Serial.println("client disonnected");
  }
}

void printWiFiStatus() {
  // print the SSID of the network you're attached to:
  Serial.print("SSID: ");
  Serial.println(WiFi.SSID());

  // print your WiFi shield's IP address:
  IPAddress ip = WiFi.localIP();
  Serial.print("IP Address: ");
  Serial.println(ip);

  // print the received signal strength:
  long rssi = WiFi.RSSI();
  Serial.print("signal strength (RSSI):");
  Serial.print(rssi);
  Serial.println(" dBm");
}

 

The problem i notice is as folloows: If the MKR100 is connected tru the USB then the device wil start if i open the serial monitor on the IDE (No Lipo attached) iget

Attempting to connect to SSID: TimeTech

SSID: TimeTech

IP Address: 192.168.178.225

signal strength (RSSI):-59 dBm

and then if i open the page in the used IP adress i get

 

analog input1 is 0.02 V

analog input3 is 3.30 V

 

Aantal meetingen vandaag: 10

Temperatuur: 29.80℃

Luchtvochtigheid: 32.80%

And the the serialmonitor  produces this output:

n

ew client

GET / HTTP/1.1

Host: 192.168.178.225

User-Agent: Mozilla/5.0 (Windows NT 10.0; WOW64; rv:54.0) Gecko/20100101 Firefox/54.0

Accept: text/html,application/xhtml+xml,application/xml;q=0.9,*/*;q=0.8

Accept-Language: nl,en-US;q=0.7,en;q=0.3

Accept-Encoding: gzip, deflate

Connection: keep-alive

Upgrade-Insecure-Requests: 1

Cache-Control: max-age=0

 

client disonnected

new client

GET / HTTP/1.1

Host: 192.168.178.225

User-Agent: Mozilla/5.0 (Windows NT 10.0; WOW64; rv:54.0) Gecko/20100101 Firefox/54.0

Accept: text/html,application/xhtml+xml,application/xml;q=0.9,*/*;q=0.8

Accept-Language: nl,en-US;q=0.7,en;q=0.3

Accept-Encoding: gzip, deflate

Connection: keep-alive

Upgrade-Insecure-Requests: 1

Cache-Control: max-age=0

Then i connect the LIPO and remove the USB connection.

If i do this the connection stays stable and present.

 

But if i remove the USB first and then plugin the LIPO then the device wont connect to the router.

 

So the question is, is this a known problem with the MKR1000 of do i something wrong in the sketch??

 

Regards

 

Harry