Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum A beginner needs help with electronics for a friend | 5 NeoPixel, 1Fan and a Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 10 answers
  • Subscribers 417 subscribers
  • Views 2404 views
  • Users 0 members are here
  • arduio
  • force sensitive resistors
  • 12v
  • buttons
  • help
  • fan
  • new
  • led
  • neopixel
  • fsr
  • 5v
  • beginner
Related

A beginner needs help with electronics for a friend | 5 NeoPixel, 1Fan and a Arduino

soxx
soxx over 9 years ago

Hello Element14 Comunity,

 

If you guys can help me, and I don't mean that you should give my a compleat circuit or code, I mean good practises or ideas and say what I have done wrong.

I am pretty mutch a beginner and I want to learn.

 

I'm building a costume for a friend and he wants LEDs and a Fan, this shouldn't be hard but I thought wrong.

(I don't know if this is even possible with an Arduino....)

 

 

So here is my idea.

 

I have an Arduino that controls 5 NeoPixel LED strips and a fan, the LEDs should change colour or in the case of the fan the speed when he presses on of the 4 Buttons, in this case, FSRs (Force Sensitive Resistors).

 

The first 3 controls the Colour with an effect of some sort.

The last one has 2 modes to manage

1. when he holds the Button down the Fan should speed up, when he presses it and holds it down again in a very short amount of time the fan should slow down to a specific speed.

2. When he just press the button all LEDs should go off or on again.

 

 

I have done the first idea in Fritzing and I don't know if this is good or the worst thing you guys have ever seen.

 

I hope you guys can help me.

 

image

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 9 years ago +3 suggested
    I would start by building the circuit in stages. Start with a single neo-pixel and add some code to just flat some colour etc. Then add the rest of the pixels and check functionality. Then the motor. Keep…
  • mcb1
    mcb1 over 9 years ago +2 suggested
    The neopixels come with some very good examples in the Adafruit library. You should be able to drive all 5 from a single regulator. https://learn.adafruit.com/adafruit-neopixel-uberguide/power gadget.iom…
  • mcb1
    mcb1 over 9 years ago in reply to niteowl12 +1 suggested
    niteowl12 Good spotting. The Sensing pin A0-A3 need to connect between the FSR and the pulldown resistor. Also PWM is only available on some pins. https://www.arduino.cc/en/Main/ArduinoBoardProMini You…
Parents
  • soxx
    0 soxx over 9 years ago

    Sooo update,

     

    mcb1:

    You could use one of those 5v power banks, and a small 12v battery just for the fan.

    It might be an easier option than trying to regulate the neopixels.

    I decided to exactly what mcb1, I will use a 5V 3A PowerBank to run theNeoPixel and Arduino and the 12Vone to run the fan.

    This is way easier to make for me right now.

     

     

    David

    PS: you can click on all pictures to get to my OneDrive with all the files.

     

    Suit%20NeoPixel%20v5_Steckplatine.png?psid=1Suit%20NeoPixel%20v5_Schaltplan.png?psid=1Suit%20NeoPixel%20v5_Leiterplatte.png?psid=1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to soxx

    I will use a 5V 3A PowerBank to run theNeoPixel and Arduino and the 12Vone to run the fan.

    Sounds a much simplier way.

     

    Your board layout has an error with Din and 5v swapped on the bottom left Neopixel, and obviously the track size needs to be much larger (never done a layout in Fritzing before)

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • soxx
    0 soxx over 9 years ago in reply to mcb1

    Your board layout has an error with Din and 5v swapped on the bottom left Neopixel

    I fixed that now, thanks.

     

     

    and obviously the track size needs to be much larger (never done a layout in Fritzing before)

     

    Oh okay, I never did a board layout bevor so thanks image

    In Fritzing I have these options for the thickness:

     

    Superthin8mil
    Extra thin12mil
    Thin2mil
    Standard24mil
    Thick32mil
    Extra thick48mil

     

    I think I need to use thick for the power and for the signals and stuff the Standart one, right?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to soxx

    I think I need to use thick for the power and for the signals and stuff the Standart one, right?

    Yes that is correct.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago in reply to soxx

    I think I need to use thick for the power and for the signals and stuff the Standart one, right?

    Yes that is correct.

     

    Mark