Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Light Switch based on Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 417 subscribers
  • Views 770 views
  • Users 0 members are here
  • arduino home automation
Related

Light Switch based on Arduino

damjan_d
damjan_d over 9 years ago

Hi,

 

I was wondering can a regular light switch be converted to a smart one, using the following requirements:

 

- No neutral wire (just one phase that goes to the lamp and from the fuse)

- The Arduino has to be always off, until WAKE event is called using photo-diode, would it wake fast enough ?

 

My goal then is to have Li-Fi based router, that will convert the web service commands from IP packets to Li-Fi signals, but first it will negotiate with the photo-diode, when it completes, the command will be processed.

 

I know this is a lot technologies patched together, however if you may answer my switch powering issue I will be more than happy image.

 

The full scale of my idea is:

- each room having the Li-Fi, rooms are identified by wi-fi AP SSID

- a device like: socket, water heater, (even fridge image) and light switch will have own ID flashed in a PIC16f* microcontroller

- a cloud service having lots of clients (android, web, etc) can view the home layout, see current state and interact with the environment

 

Thanks.

 

Regards,

Damjan.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +1 suggested
    The Arduino must be powered, but in a paused state waiting for interrupt from photo-diode to start processing. This would be very low powered. Pick another MCU if you wish lower power usage like TI launchpad…
  • awardautomation
    awardautomation over 9 years ago +1
    For some reason this picture comes to mind... in your case, the light bulb in the picture would be replaced by your arduino, and the primary winding comes from the fuse and goes to your lamp. However it…
Parents
  • clem57
    0 clem57 over 9 years ago

    The Arduino must be powered, but in a paused state waiting for interrupt from photo-diode to start processing. This would be very low powered. Pick another MCU if you wish lower power usage like TI launchpad for instance.

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    The Arduino must be powered, but in a paused state waiting for interrupt from photo-diode to start processing. This would be very low powered. Pick another MCU if you wish lower power usage like TI launchpad for instance.

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer