Arduino Forum Voltage Max on ATMEGA328 Analog Inputs?
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
  • State Verified Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 399 subscribers
  • Views 4563 views
  • Users 0 members are here
  • analog inputs arduino
Related

Voltage Max on ATMEGA328 Analog Inputs?

jw0752
jw0752 over 8 years ago

Does anyone know what the max voltage that can be applied to the analog inputs of the ATMEGA328 Arduino uP? I know that it will convert 0V to 5V but how much tolerance does it have for voltages over 5 volts?

 

Thanks

John

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +7 verified
    From the Atmega328 manual Mark
  • Problemchild
    Problemchild over 8 years ago in reply to mcb1 +3 suggested
    Amazed at the high voltage capability on the Reset...obviously expecting abuse there! One thing to note is that your signal doesn't have any transients otherwise you'll need to take those in to account…
  • shabaz
    shabaz over 8 years ago in reply to Problemchild +3 suggested
    Hi John! That may be some old-school Flash mem programming voltage pin for non-in-circuit programming. Not sure, I didn't check the datasheet, but I recall a load of Flash devices requiring 12V.
Parents
  • Problemchild
    0 Problemchild over 8 years ago

    Otherthing to note is that values over the maximum will be converted as the maximum value and the same for the minimum so inputs beyond the GND-VCC will be clipped. Some signal conditioning on your part would be required.

    Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 8 years ago

    Otherthing to note is that values over the maximum will be converted as the maximum value and the same for the minimum so inputs beyond the GND-VCC will be clipped. Some signal conditioning on your part would be required.

    Good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dougw
    0 dougw over 8 years ago in reply to Problemchild

    It sounds like if the external circuit has a high enough output impedance the protection diodes will clamp the voltage to safe levels. I would look how much current the protection diodes can handle, but I can't even handle PDFs out here in the boonies.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer