Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Smart Street Lighting based on vehicle movement detection on the LORAWAN network
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 415 subscribers
  • Views 2887 views
  • Users 0 members are here
  • smart street light
  • frontpage
  • traffic counter
  • vehicle movement
  • smart city
Related

Smart Street Lighting based on vehicle movement detection on the LORAWAN network

diliprajkumar
diliprajkumar over 8 years ago

Hi,

I am Dilip. Me and my friend are planning to do this Real-world IoT project for a graded course in our university. It can be called Smart Street Light Controller based on vehicle movement detection on the LORAWAN network.
Basically we aim to place two Arduino Vehicle movement detection kits (Arduino Nano + Proximity Sensor Shield + LoraWAN shield) on the beginning and end of a street. Whenever a vehicle crosses these sensors (i.e enters and exits a street), we want the Street Lights to Turn ON and Turn OFF as the vehicle enters and exits the street. Of course, we don’t have access to a real world street light as we don’t get permission from the city municipality office to control a real street light. But for proof of concept demonstration we plan on putting a sufficiently big, Indicator LED (Red Color) Kit (Arduino Nano + LED Kit + LoraWAN Shield) that can be controlled ON/OFF by the vehicle movement detection sensors from the LoRAWAN server/gateway. The Indicator LED needs to be preferably powered by the same power source (USB Battery Bank) that powers the Arduino or it can be self powered by means of AA batteries. The LED also needs to be sufficiently BIG and Bright, such that it should be visible if we happened to shoot it from a 10 meter distance on a iPhone Camera, so tiny breadboard LEDs won’t work for our requirement.


The main aims of the project are:

  • Turn ON a Street Light (Indicator LED) when a vehicle ENTERs a street and Turn OFF the Light when the vehicle EXITs the street
  • Measure Vehicle Count (Movement of Vehicles per day) on the road for both the left lane and right lane
  • OPTIONALLY, we would like to implement a sound sensor that turns ON a street light for a few mins when it detects unusually high noise activity


We would like to purchase all the hardware for this project from Element14, but before that can you please clarify the following:

  1. Which sensor ( UltraSonic / IR / Laser or Sound MIC sensor) is best suited for this project?
  2. Which is the best placement strategy for the sensor for measuring vehicle traffic? On top of a traffic light (facing down on the road) or on a street light or street sign pole on the side of the road?
  3. How do we segregate vehicle count on the left and right lane of the road? Can this be achieved based on effective and strategic positioning of the vehicle movement detection sensor?
  4. Which LED light (RED Color - Big, Bright, Low-Powered) can you recommend for our requirement?


We look forward for your clarifications so we can buy the right hardware and proceed in the right direction for realizing our project.

 

Best Regards,

Dilip

 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +2 suggested
    Hi Dilip, I don't have a complete answer, but you possibly want to look here for ideas that you can research further: http://www.windmill.co.uk/vehicle-sensing.html None of the methods have 100% accuracy…
  • shabaz
    shabaz over 8 years ago in reply to diliprajkumar +2
    Indeed, the detail here is what you need to focus on: All we need is a decent working system that turns a LED ON or OFF when any vehicle moves past the sensor range. I'm guessing if it were easy (by 'working…
  • genebren
    genebren over 8 years ago +2 suggested
    Greetings, A company that I worked with in the past, did something very similar to this. They built an energy saving lighting systems for parking garages. They would detect motion and turn on lights as…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Dilip,

     

    I don't have a complete answer, but you possibly want to look here for ideas that you can research further:

    http://www.windmill.co.uk/vehicle-sensing.html

    None of the methods have 100% accuracy, so you probably need to consider taking multiple data points, and also redundancy in case of hardware or software failure/error, light fixture failure and reporting, and also considerations of bicycles/motorbikes. Even with 99.9% chance of not accidentally missing a vehicle, the risk is too high, so you'll need to think up ideas for far higher accuracy. It might not be solvable (I have no idea) or you might want a different strategy (e.g. dim to 50%). These are all things you might want to consider or research for your university project. Probably there are plenty of reports from governments (this is a guess, worth investigating/googling), on risk of accidents versus light level, etc..

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • diliprajkumar
    0 diliprajkumar over 8 years ago in reply to shabaz

    Hi Shabaz,
    Thank you for your reply and valid insights. Yes we thought about dimming the LEDs too.
    We primarily aim to do data visualization on the energy savings aspect of keeping street lights dimmed or turned off.
    Accurate segregation of moving vehicles into cars and motorbikes is not the priority right now.

    All we need is a decent working system that turns a LED ON or OFF when any vehicle moves past the sensor range.
    I am not sure how detecting vehicle movement in videos will help in realtime light control, nevertheless i have contacted the Retail Sensing company you mentioned in your post.
    However if there are any other cheap sensors to get the project on track it will be nice to know!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • diliprajkumar
    0 diliprajkumar over 8 years ago in reply to shabaz

    Hi Shabaz,
    Thank you for your reply and valid insights. Yes we thought about dimming the LEDs too.
    We primarily aim to do data visualization on the energy savings aspect of keeping street lights dimmed or turned off.
    Accurate segregation of moving vehicles into cars and motorbikes is not the priority right now.

    All we need is a decent working system that turns a LED ON or OFF when any vehicle moves past the sensor range.
    I am not sure how detecting vehicle movement in videos will help in realtime light control, nevertheless i have contacted the Retail Sensing company you mentioned in your post.
    However if there are any other cheap sensors to get the project on track it will be nice to know!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to diliprajkumar

    Indeed, the detail here is what you need to focus on:

    All we need is a decent working system that turns a LED ON or OFF when any vehicle moves past the sensor range.

    I'm guessing if it were easy (by 'working' this assumes extremely high reliability for all vehicle types including bicycle, and redundancy, vehicle speed, or counting vehicles again at the egress of the controlled area to know when to reduce the lighting), then people would have installed it by now, since it is a no-brainer that the energy savings are huge.

    It isn't easy, therefore you'll need to deeply investigate, and maybe prototype up several ideas. I personally think video/image recognition or movement detection via camera has a huge part to play, but I've not explored street lighting in any detail to be sure.