Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Fischertechnik and arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 8 answers
  • Subscribers 416 subscribers
  • Views 2974 views
  • Users 0 members are here
  • arduino mega 2560
  • fischertechnik
  • electronics
  • arduino
Related

Fischertechnik and arduino

brv64
brv64 over 8 years ago

Hello!

 

I'm having a bit of trouble interfacing the Arduino with the Ultrasonic Sensor from Fichertechnik
https://content.ugfischer.com/cbfiles/fischer/Zulassungen/ft/133009-Ultrasonic-distance-sensor.pdf

Does anyone have any idea of how I could make it work?
This is the code I have so far and what I got from the oscilloscope

imageimageimageimageimageimageimageimage

 

void setup() {
  // put your setup code here, to run once:
  Serial.begin(9600);
  Serial1.begin(115200, SERIAL_8N1);
  //Serial1.begin(2400);
  pinMode(2,OUTPUT);
}


char data1 = 'a';
char data2 = 'a';


void loop() {
  // put your main code here, to run repeatedly:
  //analogWrite(2,153);
  //delay(1);
  Serial.println("Data: ");
  /*
  for(int i = 0; i < 1; i++){
    digitalWrite(2,HIGH);
    delayMicroseconds(100);
    digitalWrite(2,LOW);
    delayMicroseconds(50);
  }
  */
  
  digitalWrite(2,HIGH);
  delayMicroseconds(125);
  digitalWrite(2,LOW);
  delayMicroseconds(78);
  
  //digitalWrite(2,HIGH);
  //delayMicroseconds(90);
  //digitalWrite(2,LOW);
  
  //Serial1.print('a');
  data1 = Serial1.read();
  data2 = Serial1.read();
  Serial.println(data1,DEC);
  Serial.println(data2,DEC);
  delay(100);
}

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago in reply to beacon_dave +3 suggested
    I've tried manually writing on traces (using digital pen): But in the end it seemed a bit ugly (my handwriting isn't great!) so I just used lines/text as usual: I suppose what could be done is pull the…
  • shabaz
    shabaz over 8 years ago +2
    Hi Brandon, Please could you use the editor tools to share the oscilloscope image (with the Google drive link we have to share information before we can access it, which I at least am not comfortable with…
  • beacon_dave
    beacon_dave over 8 years ago +2
    It is a shame that the publishing date for this new book has been put back until March 2018 https://www.amazon.co.uk/dp/3864904269/_encoding=UTF8?coliid=I12JZFYLSO5E4A&colid=3C0DWEIAWWTCA&psc=0 as it would…
  • shabaz
    0 shabaz over 8 years ago

    Hi Brandon,

     

    Please could you use the editor tools to share the oscilloscope image (with the Google drive link we have to share information before we can access it, which I at least am not comfortable with and others may or may not feel the same).

     

    The question I had was, how are you handling the same-wire for transmitting the low pulse, and the received data?

     

    One easy method could be to use a transistor (as open drain or open collector) to pull the line low, although software-only methods are possible too.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago

    It is a shame that the publishing date for this new book has been put back until March 2018

    https://www.amazon.co.uk/dp/3864904269/_encoding=UTF8?coliid=I12JZFYLSO5E4A&colid=3C0DWEIAWWTCA&psc=0

    as it would have likely answered your question...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brv64
    0 brv64 over 8 years ago in reply to beacon_dave

    Thank you for the link, but it seems that it doesn't use the fischertechnik sensors.

    In my case I need the ultrasound sensor from FT, not the generic Arduino sensor.

    I'll look forward to it and learning German.

    Thank you

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brv64
    0 brv64 over 8 years ago in reply to shabaz

    It's ok, I understand.

    I added the images on the post.

    image

    I got those images by connecting the probe directly into a TXT controller and the sensor.

    If you need more images or information, please let me know

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to brv64

    Hi Brandon,

     

    I think you're not capturing the beginning part (perhaps your trigger condition needs changing, or different timebase setting), because you should see a 0.2msec delay from when you pull the line low. I can't see a 200msec delay on the traces.

    However, more concerning, is that there are multiple voltage levels in the trace, when there should only be two levels, low and high. It could be a situation where the microcontroller is functioning with (say) 3.3V logic, and the sensor is working at 5V logic levels for example. Anyway, that needs resolving, before something gets damaged. You can use logic level converters to help here.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to shabaz

    Hi Shabaz - here is what I see on the scope with a FT Robotics TXT controller and the FT ultrasonic sensor.

     

    It doesn't appear to quite match the documentation...

     

    As for the levels, the ultrasonic sensor originally was supplied with construction kits for the earlier 'TX' controllers, which were later replaced with the 'TXT' controllers. There is a blog about inside the TX controller here:

    Hacking the Fischertechnik TX Controller - Stefan Brunner

     

    image

     

    image

     

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to beacon_dave

    Hi Dave,

     

    Great captures! I just had a look at the URL you mentioned, the controllers look really sophisticated!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to shabaz

    I'm starting to wonder if my captures are inverted...

     

    Doesn't really help with the signal being on a black wire with a red connector, and the ground on red/green wire with a green connector... At least the power is on a red wire with a red connector.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to shabaz

    The specification for the newer TXT controller can be found at:

    https://www.fischertechnik.de/en/products/playing/robotics/522429-robotics-txt-controller

    Similar form factor but it is based around a dual processor ARM Cortex A8 (32bit/600mHz) + Cortex M3

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to beacon_dave

    I had another look at this and it is starting to make sense now. The timings appear to be a bit out compared to the documentation though.

     

    This screenshot shows two 'host queries'. The first query doesn't get a response from the sensor (not mandatory) but presumably causes an ultrasonic 'TX Burst' at the sensor. The second around 10ms later, with the 'RX Response' data supplied in two bytes, high first, then the low. 

     

    image

     

     

     

    This screenshot shows the second 'Host Query' in more detail. The low pulse from the controller is around 44us rather than the documented 78us. The '2-Byte answer' is a bit quicker than the documented 0.2ms - 1ms. The high byte shows a value of 0x80 with only bit D7 set indicating it is the 'first byte'. The low byte shows a value of 0x09 with only bits D0 and D3 set. This distance value corresponds with the value displayed in the control software.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>