Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum My first electronics project, and it's a BIG one
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 13 answers
  • Subscribers 417 subscribers
  • Views 4139 views
  • Users 0 members are here
  • diy
  • midi
Related

My first electronics project, and it's a BIG one

cdog580
cdog580 over 8 years ago

hello everyone this is my first post and i am very new at electronics. i am a lighting designer that designs and programs lights for concerts and other events. my preferred console that i use is a grand MA2 software and i have a on pc command wing. I have always found electronics fascinating and now that i have the following issue i have decided now is a perfect time to start! here is the project:

 

i am attempting to make a replica of this fader wing extension which retail cost over $3,500 easy. for my project i need to meet the following:

 

15 x 60mm linear slide potentiometers

60 x cherry MX white switches

USB type B connection to control the hardware via midi control.

 

the things i would like to do are this:

1) prototype and ensure that the entire system is working

2) program a stand alone pcb mounted microcontroller to control the hardware and software interactions preferably without using a arduino or similar thought this may be selfish?

3) have a proper PCB and Metal housing cut so that i am able to use it on actual jobs.

my big question is this:

what do you all recommend for me as a starting point. i can do the research on the potentiometers and the buttons thought those seem easy enough. have the microcontroller listening for the voltage of the potentiometers and for the buttons to send it 5 volts but i know there is no microcontroller that will have the whole 75 inputs i will need. do i use multiple microcontrollers? how do i hook them together? is there something i am missing in this project? thank you all for any input!

 

***********************

*       UPDATE        *

***********************

 

so i have discovered that there is a arduino Mega which has 50 odd connections not the full 75 i need but if there's a way to link the two and then have one USB out to the computer this may solve my issue of lack of i/o ports and dramatically reduce the complexity of this project.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Chris, This is a quite ambitious project especially if you are going to try to design it yourself. The people who can design sophisticated systems usually go to school for it for years and spend most…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Chris, This is where you might use a multiplexer A multiplexer is switch that can set to select one of it's inputs and connect it to it's output The output of the multiplexer would attach to one of…
  • cdog580
    cdog580 over 8 years ago in reply to jw0752 +2
    yea i figured it was going to be a big project. making one row of them is easy enough but to make 15 sets of 5 different parts is definitely going to be a task! maybe making these into modules of 5 faders…
Parents
  • genebren
    0 genebren over 8 years ago

    Hi Chris,

     

    This is where you might use a multiplexer A multiplexer is switch that can set to select one of it's inputs and connect it to it's output The output of the multiplexer would attach to one of the ADC inputs of the microprocessor(most likely also using a multiplexer to route one of the inputs to an ADC The select lines for the multiplexers(yes you might need a couple of mux's will be driven from the microprocessor to make the necessary selections A suitable part might be an  74HC4051D74HC4051D which is an 8 to 1 multiplexer

     

    This is a pretty straight forward approach for reading several inputs with a single microprocessor.  I have used this on several projects.  The microprocessor could use a timer interrupt to manage all of the sampling of your controls (switches and pots).  The logic could be something like this:

    • 1st interrupt - drive all mux's to input 1, set ADC to first Mux.
    • 2nd interrupt - start ADC
    • 3rd interrupt - read ADC, set ADC to next Mux.
    • repeat steps 2 and 3 until all of the external Mux input 1have been read.
    • advance external mux's to imput 2, set ADC to first Mux.
    • repeat until all inputs have been sampled.

    This process would run continuously sampling all of the pots and switches in the background.  Once all of the data is collected and saved in RAM, the timer routine would set a flag the would indicate to the maim program that the data is ready to be processed.

     

    I hope this helps!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to genebren

    time to start researching those haha i knew this was going to be a challenge but it seemed like it was just scaling a small project. might have miss-judged that a little haha. if you have any input on the reply i wrote to john i would be very appreciative of any input. thank you again for your reply!

     

    -chris

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to cdog580

    Chris,

     

    Building your project as a series of smaller boards may also help.  By having something like 5 boards of 3 pot and 12 switches or 3 boards 5 pots and 20 switches might make the project more manageable.  These boards could be designed such that the pots and switches could mount directly to the boards (much less wiring).  The boards could either have their own microprocessors or each be controlled by an Arduino.  With a multiple board approach you would need to have a way to communicate between the boards (serial, I2C, etc) and one of the boards would have to host the USB to the PC (master, with the other boards being slaves).

     

    A couple of things to keep in mind:

    • Only the the pot inputs need to be read by the ADC.
    • The switches can be configured such that they can be read by a standard I/O pin (digital).

     

    Anything is possible, just break things down into simple steps.  Start by using breadboards, an do simple things like reading a pot, or a switch.  Only once you understand how to do each fundamental step should you begin to start laying out the bigger design.

     

    Best of luck, and enjoy the journey!

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to genebren

    Thank you gene for your input! Am I correct in thinking that I can use the arduino to program the microprocessor and then just remove it and mount it to the pcb? Then use ribbon cable or something to connect each pcb together. I would assume that for the main processor and the USB I could use a regular arduino for my main input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to cdog580

    Chris,

     

    If you are using a microprocessor other than the Arduino, there are simpler approaches to programming.  Most microprocessors can be programmed on the board, through a simple plugin programmer (usually a 6-pin header is all that is needed).  This good to have, as it might take a bit of work to get it all working, so being able tr reprogram is a great thing. As far as the main processor, i assume that an arduino should work (I personally do not have a lot of ardunio experience).

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago in reply to cdog580

    Chris,

     

    If you are using a microprocessor other than the Arduino, there are simpler approaches to programming.  Most microprocessors can be programmed on the board, through a simple plugin programmer (usually a 6-pin header is all that is needed).  This good to have, as it might take a bit of work to get it all working, so being able tr reprogram is a great thing. As far as the main processor, i assume that an arduino should work (I personally do not have a lot of ardunio experience).

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer