Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum My first electronics project, and it's a BIG one
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 13 answers
  • Subscribers 417 subscribers
  • Views 4157 views
  • Users 0 members are here
  • diy
  • midi
Related

My first electronics project, and it's a BIG one

cdog580
cdog580 over 8 years ago

hello everyone this is my first post and i am very new at electronics. i am a lighting designer that designs and programs lights for concerts and other events. my preferred console that i use is a grand MA2 software and i have a on pc command wing. I have always found electronics fascinating and now that i have the following issue i have decided now is a perfect time to start! here is the project:

 

i am attempting to make a replica of this fader wing extension which retail cost over $3,500 easy. for my project i need to meet the following:

 

15 x 60mm linear slide potentiometers

60 x cherry MX white switches

USB type B connection to control the hardware via midi control.

 

the things i would like to do are this:

1) prototype and ensure that the entire system is working

2) program a stand alone pcb mounted microcontroller to control the hardware and software interactions preferably without using a arduino or similar thought this may be selfish?

3) have a proper PCB and Metal housing cut so that i am able to use it on actual jobs.

my big question is this:

what do you all recommend for me as a starting point. i can do the research on the potentiometers and the buttons thought those seem easy enough. have the microcontroller listening for the voltage of the potentiometers and for the buttons to send it 5 volts but i know there is no microcontroller that will have the whole 75 inputs i will need. do i use multiple microcontrollers? how do i hook them together? is there something i am missing in this project? thank you all for any input!

 

***********************

*       UPDATE        *

***********************

 

so i have discovered that there is a arduino Mega which has 50 odd connections not the full 75 i need but if there's a way to link the two and then have one USB out to the computer this may solve my issue of lack of i/o ports and dramatically reduce the complexity of this project.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Chris, This is a quite ambitious project especially if you are going to try to design it yourself. The people who can design sophisticated systems usually go to school for it for years and spend most…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Chris, This is where you might use a multiplexer A multiplexer is switch that can set to select one of it's inputs and connect it to it's output The output of the multiplexer would attach to one of…
  • cdog580
    cdog580 over 8 years ago in reply to jw0752 +2
    yea i figured it was going to be a big project. making one row of them is easy enough but to make 15 sets of 5 different parts is definitely going to be a task! maybe making these into modules of 5 faders…
  • e14phil
    0 e14phil over 8 years ago

    .. side note... An Alternative to Arduino>Midi is:   

     

    Arduino>HID>USB>MidiYoke>Midi

    https://www.arduino.cc/en/Reference/HID .

     

    That way you can have multiple input devices.

     

    Phil  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to e14phil

    thank you for your suggestion i will take a look!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to beacon_dave

    i was thinking about putting in motorized faders but then i realized how many I/O pins i am using. the one that i am replicating does not have motorized fader, though the ones for their mainstream consoles do. the reason for the high price isn't the hardware as much as it is parameters. in order to control the light you need their hardware that contains a special handshake which allows the piece of hardware to "unlock" parameters. a parameter in the software could be something like color, pan, tilt, intensity, etc. that is where the big money comes into play. i own a command wing which already gives me 2048 parameters which is more than plenty for my application. on their lite console they have 15 faders and "executors" which are very handy to have hardware buttons to control them. that's kinda where this whole idea started was i just wanted to have physical buttons to press.

    their console fader wing has motorized faders but this piece of hardware is $7,600

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<