Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum My first electronics project, and it's a BIG one
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 13 answers
  • Subscribers 417 subscribers
  • Views 4152 views
  • Users 0 members are here
  • diy
  • midi
Related

My first electronics project, and it's a BIG one

cdog580
cdog580 over 8 years ago

hello everyone this is my first post and i am very new at electronics. i am a lighting designer that designs and programs lights for concerts and other events. my preferred console that i use is a grand MA2 software and i have a on pc command wing. I have always found electronics fascinating and now that i have the following issue i have decided now is a perfect time to start! here is the project:

 

i am attempting to make a replica of this fader wing extension which retail cost over $3,500 easy. for my project i need to meet the following:

 

15 x 60mm linear slide potentiometers

60 x cherry MX white switches

USB type B connection to control the hardware via midi control.

 

the things i would like to do are this:

1) prototype and ensure that the entire system is working

2) program a stand alone pcb mounted microcontroller to control the hardware and software interactions preferably without using a arduino or similar thought this may be selfish?

3) have a proper PCB and Metal housing cut so that i am able to use it on actual jobs.

my big question is this:

what do you all recommend for me as a starting point. i can do the research on the potentiometers and the buttons thought those seem easy enough. have the microcontroller listening for the voltage of the potentiometers and for the buttons to send it 5 volts but i know there is no microcontroller that will have the whole 75 inputs i will need. do i use multiple microcontrollers? how do i hook them together? is there something i am missing in this project? thank you all for any input!

 

***********************

*       UPDATE        *

***********************

 

so i have discovered that there is a arduino Mega which has 50 odd connections not the full 75 i need but if there's a way to link the two and then have one USB out to the computer this may solve my issue of lack of i/o ports and dramatically reduce the complexity of this project.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Chris, This is a quite ambitious project especially if you are going to try to design it yourself. The people who can design sophisticated systems usually go to school for it for years and spend most…
  • genebren
    genebren over 8 years ago +3 suggested
    Hi Chris, This is where you might use a multiplexer A multiplexer is switch that can set to select one of it's inputs and connect it to it's output The output of the multiplexer would attach to one of…
  • cdog580
    cdog580 over 8 years ago in reply to jw0752 +2
    yea i figured it was going to be a big project. making one row of them is easy enough but to make 15 sets of 5 different parts is definitely going to be a task! maybe making these into modules of 5 faders…
  • genebren
    0 genebren over 8 years ago in reply to cdog580

    Chris,

     

    If you are using a microprocessor other than the Arduino, there are simpler approaches to programming.  Most microprocessors can be programmed on the board, through a simple plugin programmer (usually a 6-pin header is all that is needed).  This good to have, as it might take a bit of work to get it all working, so being able tr reprogram is a great thing. As far as the main processor, i assume that an arduino should work (I personally do not have a lot of ardunio experience).

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to cdog580

    Yes indeed but you may need a few additional support components such as a crystal if not using the internal resonator.

     

    Keep in mind that the likes of an Arduino Uno is based around the ATmega328 microcontroller with a few additional peripherals such as clock voltage regulator USB to  RS-232RS-232 interface etc Perhaps take a look at this tutorial to see how to build one on breadboard

    https://www.arduino.cc/en/Main/Standalone

     

    The ATmega328 supplied in the Uno has an Arduino bootloader loaded onto it which then allows Arduino sketches to be loaded onto it via the Ardunio IDE to run you programs.

     

    You can use an Arduino as a programmer to program stock AVR microcontrollers (which don't have the Arduino bootloader loaded). Take a look here for more information:

    https://www.arduino.cc/en/Tutorial/ArduinoToBreadboard

     

     

    The likes of the ATmega328 microcontroller can also be programmed outside of the Arduino IDE environment using something like Atmel Studio 7.  This also gives you access to a much wider range of microcontrollers if you want the flexibility. Take a look at some of the other microcontrollers available in the AVR family:

    Atmel AVR 8-bit and 32-bit Microcontrollers

     

    The Arduino platform is however an excellent starting point for prototyping due to all the support (books, web pages, forums) that surrounds it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago

    I also agree with the sentiment expressed by everyone, to start in smaller chunks. From the URL you linked, it is unclear what the protocol is over USB to the PC software. Is it USB-MIDI, or is it some proprietary protocol between the PC software and the off-the-shelf controller? Also, even if it is MIDI, the traffic would need to be examined to see precisely what information is going over that link, like what channel, instrument number, etc I'm guessing. This is if you're looking for compatibility between that software and your hardware attachment.

    Some prototype code should be written (it could be done before even drawing a circuit or PCB), to simulate your input from a fader, and to send the value over the USB connection, receive over the USB connection and send to the DMX connection perhaps. I didn't really understand the flow, is it that the MIDI input is on the hardware device you wish to create, then send the data to the PC via USB, which manipulates it to control a lighting channel in conjunction with the fader setting, and then sends it back to the hardware you wish to create, to output over the DMX connection?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to shabaz

    the software allows you to map the midi channels to whatever i would like. It would receive and send data back to the controller over USB. what i have learned from the answers of the people above i have decided to possibly approach the project as follows: i will use 3 separate PCBs that will have 5 potentiometers and 20 cherry MX clear switches as well as a LED for each switch. i am currently working on a schematic which i will post soon. i would like to document this journey as i think eventually it may be useful to many people. i will have the PCBs hook up to a arduino mega and one other board but i haven't decided which one yet because if i use a mega i will be short by only 6 digital I/O pins for switches. maybe the ATxmega128A1U? to replace it all. the biggest challenge i see for this project is getting the single, or multiple, micro controllers to communicate properly as well as having the boards communicate with the pc over USB and actually get the midi signal channels to be correct so that in the software i can map them without too much trouble. let me know what you think about this and thank you for your input!

    -chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to cdog580

    You can perhaps reduce the digital IO pin count required by arranging the switches in an 8 by 8 grid. That way with 16x IO pins on the microcontroller, you can read the state of up to 64 switches.

     

    You could also perhaps use external shift registers to reduce the pin count required without going to multiple micro controllers. 

     

    Your LED's may be a bit harder though if you want to vary the brightness levels between on and off, as you are likely to want PWM enabled outputs for that (and not all digital IO is PWM enabled). Alternatively you could perhaps use pixel LED's, which would allow you to drive all 60 switch LED's from one or two IO pins.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to beacon_dave

    Interesting thought. I could do the matrix idea to cut down on the use of pins. I may still need a mega though as there are 3 sections of 5 faders where each fader has 4 3 associated buttons. The bottom row of buttons does something different.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to cdog580

    The Arduino Mega gives you 4x hardware USARTs as well, just in case you want to replicate the functionality of the DMX512 XLR outputs.

     

    Note that only 15 pins of the Mega 2560's IO can be assigned to PWM use to allow you to vary LED brightness. However as previously mentioned you could perhaps use pixel LEDs which have built in PWM control instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cdog580
    0 cdog580 over 8 years ago in reply to beacon_dave

    The manufacturer has had issues with Chinese replicas stealing parameters which allow the lights to be controlled. That’s why I only want to make a midi controller because I like and respect the manufacturer and I don’t really need more parameters

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 8 years ago in reply to cdog580

    Just a passing thought but are the faders on the fader wing motorised (perhaps reflecting the cost) ?

     

    If so, then you will likely need an additional couple of outputs to drive an H-bridge motor controller along with an additional input for the capacitive touch sensing (although I guess the touch sense could disable the H-bridge directly if you aren't using interrupts).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14phil
    0 e14phil over 8 years ago

    Hi Chris

     

    I have previously watched this Arduino to Midi series.

    https://www.youtube.com/watch?v=DXhxdsGREsU

     

    I would suggest it as a starting point.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<>