Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Please I need help Writing code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 51 replies
  • Answers 9 answers
  • Subscribers 420 subscribers
  • Views 6305 views
  • Users 0 members are here
  • need help coding
  • need code written
Related

Please I need help Writing code

theshay
theshay over 8 years ago

I am trying to write code for an automatic railroad crossing gates for my grandsons train table i built. I have no clue what i am doing. What i can say is im using 2 servos with external power 4 red leds that need to flash and a speaker for bell ding which i was hoping to use a sound file to play back my wire config is 2,3 for leds  2 servos 5,6 I also have a 10 second record-able device for train horn which uses push button for playback. i wanted to cut off the push button and use the arduino r3 to act as the push button pin 8. Also i will have 2 reed switches one to activate gates and lights and one to deactivate pins 4,7 this is what i have so far I get the lights to flash but im lost from there can some one help me write this code?

 

@@@@

int rd1LEDPin=2; //Declares rd1LED as int and set to 2

int rd2LEDPin=3; //declairs rd2LED as int and set to 3

 

int rd1onTime=250; //light 1 on time

int rd1offTime=250;  // light 1 off time

int rd2onTime=250; //light 2 on time

int rd2offTime=250;  // light 2 off time

 

const int REED_PIN = 4; // Pin connected to reed switch

const int REED_PIN = 7; // Pin connected to reed switch

const int LED_PIN = 13; // LED pin - active-high

 

 

void setup() {

  pinMode(rd1LEDPin, OUTPUT);// sets the second pin for output

   pinMode(rd2LEDPin, OUTPUT);// sets the third pin for output

 

  Serial.begin(9600);

  // Since the other end of the reed switch is connected to ground, we need

  // to pull-up the reed switch pin internally.

  pinMode(REED_PIN, INPUT_PULLUP);

  pinMode(LED_PIN, OUTPUT);

}

 

void loop() {

  digitalWrite(rd1LEDPin,HIGH); //turns led 1 on

  digitalWrite(rd2LEDPin,LOW); // turns led 2 off

  delay (rd1onTime); //wait

  delay(rd2offTime); //wait

 

  digitalWrite(rd1LEDPin,LOW); //turns led 1 off

  digitalWrite(rd2LEDPin,HIGH);//turns led 2 on

  delay (rd1offTime);//  wait

  delay(rd2onTime);  //wait

 

  int proximity = digitalRead(REED_PIN); // Read the state of the switch

  if (proximity == LOW) // If the pin reads low, the switch is closed.

  {

    Serial.println("Switch closed");

    digitalWrite(LED_PIN, HIGH); // Turn the LED on

  }

  else

  {

    digitalWrite(LED_PIN, LOW); // Turn the LED off

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • theshay
    theshay over 8 years ago in reply to andywest +4 suggested
    ok i changed it. please for give me im an old man trying to do something for my autistic grandson he loves trains. so i build him a table for his birthday. only thing left to do is make the crossing gates…
  • jomoenginer
    jomoenginer over 8 years ago in reply to theshay +3 suggested
    Considering your lack of code development background, gabbing code examples might be causing more of an issue for you than it may solve. My suggestion for you is to write out what you want the code to…
  • theshay
    theshay over 8 years ago in reply to balearicdynamics +3
    Thank you so very much Enrico You are truly an honor and a scholar. May the guiding light be with you! I cant thank you enough for helping me. you really got me out of a jam. :-))) Not sure if you travel…
Parents
  • balearicdynamics
    0 balearicdynamics over 8 years ago

    Hello Edward,

     

    I am sorry to miss your question, thanks to tariq.ahmad  now I am on the piece image Don't worry we can easily solve your problem; BTW, maybe many users say that the problems are easy. I always found easy the problems I already know the solution image

     

    I ask you a favor, please. Take a look in the editor features and add the code with Syntax Highlighting so I can easily copy and past it in one Arduino board here to make some test and solve it faster. It was my browser rendering wrond your sources, now I can see them correctly. So, go ahead.

     

    As far as I see lights may flash with your code but this approach IMHO may create difficulties implementing the other part, better if we use a couple of separate functions. Let me know as I am almost available to follow you these days.

     

    Wait for your code to try it together. image What is the Birthday deadline?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to balearicdynamics

    As waiting for your code I mean your last update after the mcb1 suggestions eventually applied.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    [code]
    /*
    Railroad crossing controller
    */
    #include 
    
    // Constants
    const int CYCLE_PERIOD_MS = 10;
    
    const int SENSOR_DELTA_THRESHOLD = 20;
    
    const int BELL_RING_PERIOD = 400;
    const int BELL_RING_CYCLES = BELL_RING_PERIOD / CYCLE_PERIOD_MS;
    const int BELL_TONE_FREQUENCY = 300;
    const int BELL_DURATION = 180;
    
    const int LIGHT_BLINK_PERIOD = 1000;
    const int LIGHT_BLINK_CYCLES = LIGHT_BLINK_PERIOD / CYCLE_PERIOD_MS;
    const int LIGHT_BLINK_HALF_CYCLES = LIGHT_BLINK_CYCLES / 2;
    
    const float CROSSING_POSITION_RAISED = 110.0;
    const float CROSSING_POSITION_LOWERED = 15.0;
    const float CROSSING_DEGREES_PER_CYCLE = 0.1;
    
    const int TRAIN_SPEED_MS_PER_SECTION = 1000;
    const int TRAIN_SECTIONS_TO_CROSSING = 13;
    
    const int TIME_GATE_WARNING_BEFORE_TRAIN_MS = 7000;
    const int TIME_GATE_DOWN_BEFORE_TRAIN_MS = 5000;
    const int TIME_GATE_DOWN_AFTER_TRAIN_MS = 2000;
    const int TIME_GATE_DOWN_BEFORE_TRAIN_CYCLES = TIME_GATE_DOWN_BEFORE_TRAIN_MS / CYCLE_PERIOD_MS;
    const int TIME_GATE_DOWN_AFTER_TRAIN_CYCLES = TIME_GATE_DOWN_AFTER_TRAIN_MS / CYCLE_PERIOD_MS;
    
    const int PIN_SENSOR = 0;
    const int PIN_LEFT_LIGHT = 2;
    const int PIN_RIGHT_LIGHT = 3;
    const int PIN_STATUS_LIGHT_ARRIVAL = 4;
    const int PIN_STATUS_LIGHT_DEPARTURE = 5;
    const int PIN_BUZZER = 6;
    const int PIN_SERVO = 7;
    
    // Enums and globals
    enum sensorState {
      out, entering, in, exiting
    }
    sensorState = out;
    
    enum crossingState {
      up, warning, lowering, down, raising
    }
    crossingState = up;
    
    Servo gateServo;
    int sensorThreshold = 0;
    long trainArrivalCountDownMS = 0;
    long trainDepartureCountDownMS = 0;
    int bellCycleCounter = 0;
    int leftLightCycleCounter = 0;
    int rightLightCycleCounter = LIGHT_BLINK_HALF_CYCLES;
    float crossingPosition = CROSSING_POSITION_RAISED;
    
    
    /*
    One time initializations
    */
    void setup()
    {
      pinMode(PIN_LEFT_LIGHT, OUTPUT);
      pinMode(PIN_RIGHT_LIGHT, OUTPUT);
      pinMode(PIN_STATUS_LIGHT_ARRIVAL, OUTPUT);
      pinMode(PIN_STATUS_LIGHT_DEPARTURE, OUTPUT);
      pinMode(PIN_BUZZER, OUTPUT);
     
      // we assume that a train is not in the sensor at startup
      sensorThreshold = analogRead(PIN_SENSOR) + SENSOR_DELTA_THRESHOLD;
    
      gateServo.attach(PIN_SERVO);
      gateServo.write(CROSSING_POSITION_RAISED);
    
      Serial.begin(9600);
    }
    
    /*
    Main control loop.
    Check the sensor, update outputs, and then wait the cycle period.
    */
    void loop()
    {
      checkSensor();
      updateTimers();
      updateStatusLights();
      updateCrossingState();
      updateBells();
      updateLights();
      updateGatePosition();
      delay(CYCLE_PERIOD_MS);
    }
    
    
    /*
     Check sensor and update transitions or states
     */
    void checkSensor()
    {
      if (isTrainPresentAtSensor()) {
        switch (sensorState) {
          case in:
            // still in...
            break;
          case entering:
            Serial.println("\nsensor -> in");
            sensorState = in;
            break;
          case out:
          case exiting:
            Serial.println("\nsensor -> entering");
            sensorState = entering;
            break;
        }
      } else {
        switch (sensorState) {
          case in:
          case entering:
            Serial.println("\nsensor -> exiting");
            sensorState = exiting;
            break;
          case out:
            break;
          case exiting:
            Serial.println("\nsensor -> out");
            sensorState = out;
            break;
        }  
      }
    }
    
    /*
     Set the timers when a train arrives,
     increment the departure timer if a train is still in the sensor,
     decrement the timers if a train is on its way
     */
    void updateTimers() {
      switch (sensorState) {
        case in:
          trainDepartureCountDownMS += CYCLE_PERIOD_MS;
          break;
        case entering:
          // is this a new train or an additional train?
          if (trainDepartureCountDownMS > 0) {
            // it is an additional train...
            // leave the arrival time as-is, add the time it takes for the new train to arrive on the departure timer
            Serial.println("\nAdditional train detected...");
            trainDepartureCountDownMS = calculateTrainArrivalTimeMS() + CYCLE_PERIOD_MS + TIME_GATE_DOWN_AFTER_TRAIN_MS;  
            // Serial.print("Arrival: ");
            // Serial.print(trainArrivalCountDownMS);
            // Serial.print("Departure: ");
            // Serial.println(trainDepartureCountDownMS);  
          } else {
            // it is a new train...
            Serial.println("\nNew train detected...");
            trainArrivalCountDownMS = calculateTrainArrivalTimeMS();
            trainDepartureCountDownMS = trainArrivalCountDownMS + CYCLE_PERIOD_MS + TIME_GATE_DOWN_AFTER_TRAIN_MS;
            // Serial.print("Arrival: ");
            // Serial.print(trainArrivalCountDownMS);
            // Serial.print("Departure: ");
            // Serial.println(trainDepartureCountDownMS);  
          }
          break;
        case out:    
        case exiting:
         // do nothing additional
         break;
      }
     
      if (trainArrivalCountDownMS > 0) {
        trainArrivalCountDownMS -= CYCLE_PERIOD_MS;
      }
     
      if (trainDepartureCountDownMS > 0) {
        trainDepartureCountDownMS -= CYCLE_PERIOD_MS;
      }
    }
     
    
    /*
     Manage crossing state transitions
     */
    void updateCrossingState() {
      switch (crossingState) {
        case up:
          if ((trainDepartureCountDownMS > 0) && (trainArrivalCountDownMS < TIME_GATE_WARNING_BEFORE_TRAIN_MS)) {
            Serial.println("\ngate up -> warning");
            crossingState = warning;
          }
          break;
        case warning:
          if (trainArrivalCountDownMS < TIME_GATE_DOWN_BEFORE_TRAIN_MS) {
            Serial.println("\ngate warning -> lowering");
            crossingState = lowering;
          }
          break;
        case lowering:
          if (crossingPosition <= CROSSING_POSITION_LOWERED) {
            Serial.println("\ngate lowering -> down");
            crossingState = down;      
          } else {
            crossingPosition -= CROSSING_DEGREES_PER_CYCLE;
          }
          break;
        case down:
          if (trainDepartureCountDownMS <= 0) {
            Serial.println("\n(expected train departure from gate)");
            Serial.println("\ngate down -> raising");
            crossingState = raising;
          }
          break;
        case raising:
          if (crossingPosition >= CROSSING_POSITION_RAISED) {
            Serial.println("\ngate raising -> up");
            crossingState = up;      
          } else {
            crossingPosition += CROSSING_DEGREES_PER_CYCLE;
          }
          break;
      }
    }
    
    
    
    /*
    We have one light to show the arrival countdown timer > 0 and
    another light to show the departure countdown timer > 0
     */
    void updateStatusLights() {
      if (trainArrivalCountDownMS > 0) {
        digitalWrite(PIN_STATUS_LIGHT_ARRIVAL, HIGH);
      } else {
        digitalWrite(PIN_STATUS_LIGHT_ARRIVAL, LOW);
      }
      
      if (trainDepartureCountDownMS > 0) {
        digitalWrite(PIN_STATUS_LIGHT_DEPARTURE, HIGH);
      } else {
        digitalWrite(PIN_STATUS_LIGHT_DEPARTURE, LOW);
      }
    }
    
    
    /*
    Helper to determine if the train is in the sensor
    */
    boolean isTrainPresentAtSensor() {
      int sensorValue = analogRead(PIN_SENSOR);
      // Serial.println(sensorValue);
      if (analogRead(PIN_SENSOR) > sensorThreshold) {
        Serial.print("S");
        return true;
      } else {
        return false;
      }
    }
    
    /*
    We do a very simplistic calculation with the assumption that all
    trains move at the same speed.  If we had a better sensor we could
    figure out how fast an individual train was going
    */
    int calculateTrainArrivalTimeMS() {
      return TRAIN_SPEED_MS_PER_SECTION * TRAIN_SECTIONS_TO_CROSSING;
    }
    
    
    /*
    Bells only ring during the initial warning and
    when the gate is lowering
    */
    void updateBells()
    {
      switch (crossingState) {
        case warning:
        case lowering:
          if (bellCycleCounter == 0) {
            Serial.print("(B!)");
            tone(PIN_BUZZER, BELL_TONE_FREQUENCY, BELL_DURATION);
            bellCycleCounter = BELL_RING_CYCLES;
          } else {
            bellCycleCounter--;
          }
          break;
      }
    }
    
    
    /*
    Lights flash continuously when the gate is not up
    */
    void updateLights()
    {
      switch (crossingState) {
        case up:
          digitalWrite(PIN_LEFT_LIGHT, LOW);
          digitalWrite(PIN_RIGHT_LIGHT, LOW);
          break;
        case warning:
        case lowering:
        case down:
        case raising:
          if (leftLightCycleCounter == 0) {
            Serial.print("(LL)");
            digitalWrite(PIN_LEFT_LIGHT, HIGH);
            digitalWrite(PIN_RIGHT_LIGHT, LOW);
            leftLightCycleCounter = LIGHT_BLINK_CYCLES;
            rightLightCycleCounter--;
          } else if (rightLightCycleCounter == 0) {
            Serial.print("(RL)");
            digitalWrite(PIN_LEFT_LIGHT, LOW);
            digitalWrite(PIN_RIGHT_LIGHT, HIGH);
              rightLightCycleCounter = LIGHT_BLINK_CYCLES;
            leftLightCycleCounter--;
          } else {
            leftLightCycleCounter--;
            rightLightCycleCounter--;
          }
          break;
      }
    }
    
    /*
    Manage incremental changes to the servo position
    */
    void updateGatePosition()
    {
      switch (crossingState) {
         case lowering:
           if (crossingPosition > CROSSING_POSITION_LOWERED) {
             crossingPosition -= CROSSING_DEGREES_PER_CYCLE;
             gateServo.write(crossingPosition);  // Move to next position
           }
           break;
         case raising:
           if (crossingPosition < CROSSING_POSITION_RAISED) {
             crossingPosition += CROSSING_DEGREES_PER_CYCLE;
             gateServo.write(crossingPosition);  // Move to next position
           }
           break;
      }
    }
    [/code]

    this is the code i found that i would like to altar to my needs but unsure how to do it i have no coding experience I can tell you where i have things plugged but not sure how to altar to my needs

    pin 2,3 are the leds pins 5.6 are servo pin 9 to act as switch to activate external sound card pins 4,7 will be the reed switches servos have external powersource

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to theshay

    oh and the birthday is may second.Thats why im freaking out to get this finished i have been building the table for 3 months its down to the finishing touches, applying trees and detail and getting these crossing gates to work. I tried going through a few tutorials an how to code but i cant learn fast enough. Its tough to teach an old dog new tricks. LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • theshay
    0 theshay over 8 years ago in reply to theshay

    oh and the birthday is may second.Thats why im freaking out to get this finished i have been building the table for 3 months its down to the finishing touches, applying trees and detail and getting these crossing gates to work. I tried going through a few tutorials an how to code but i cant learn fast enough. Its tough to teach an old dog new tricks. LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to theshay

    Ok, I should finish something before then this evening I will try to put your code on Arduino and see what it does.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    Enrico,

         Not sure if you had a chance to look at the new code and schematic I posted. I think it would be easier to modify because it is closest to what i am looking for. it only needs the switches added. Unfortunately Ive been trying to figure it out myself but just not getting it. Everyone has advice but I don't think they understand I know nothing about writing code. I wish i had more time to learn, going forward I will be doing more tutorials Because I really like the possibilities of the Arduino system and am interested in learning but for now im in a jam. I appreciate any and all help you can give me. Again I would like to thank you for your time, as I'm sure you have better things to do.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to theshay

    Hello Edward,

     

    here it is midnight. I should solve a problem of mine then I will check your source to my Arduino. I think I can do it tomorrow morning...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    Enrico,

         Ok I really appreciate you helping me. I wasn't for sure if you had seen the new stuff i posted. it is 6:30pm here im usually up all nite as I am retired. I will post some pics of the table and a video once I get it operating correctly. I am currently running all my wire for lights ect.. servos and crossing lights are already ran just need to hook to Arduino.Again I thank you very much and look forward to hearing from you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to theshay

    Great! Really, a nice scenario image I finally I am closing my stuff tonight and thanks God tomorrow morning I can put your code on an Arduino, then test what's happens. I hope I have not delayed too much and this can be helpful to you.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 8 years ago in reply to theshay

    Edward,

     

    That is a great setup you have there.

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    Enrico,

         No problem brother I appreciate your help. still plenty of time i have almost two weeks to finish up. I ordered a few more things off line to add they should be here by the weekend. I am adding camping tents and campers around the two fire pits, one is on the mountain looks like a black circle, it is actually lighted just not wired yet. to wire everything will only take me 1 day, I also ordered more street lights to put around the track those are all working lights too just like the ones in the beach parking lot. the empty corner to the lower right is where the petrol station is going. I am building that with foam core board and printed designs. All of the grass is stained saw dust instead of spending 30 bucks or more just for fake grass. trees are branches cut from a bush and glued deer moss and painted. The reeds along the lake side are chip brushes taken apart then glued the bristles into clusters.  All of the miniature people I ordered off wish.com for 2 bucks free shipping. Arduino card from wish for 5 bucks and a clear case for Arduino 2 bucks on wish. The street lamps I got 20 for 10 bucks on wish.comThe parking-lot and roads are printed then glued on foam core. The power to run everything with plenty of add on room is a 200watt computer supply converted into 3v, 5, 12v outputs all packed neatly into a service box used to be old fuse box for my garage. the train, not all shown I have had since the mid 80's. The slot car track I bought 2 years ago for my grandson to play with when he visits. He keeps asking me where it is and can he play with it. I,m so excited I can't wait to see the look on his face when he sees what grandpa has made for him. :-))

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • theshay
    0 theshay over 8 years ago in reply to balearicdynamics

    the servos did not work and i need to add 2 reed switches 1 for on 1 for off also i need to activate a sound card with a relay