Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum HELP PLS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 417 subscribers
  • Views 809 views
  • Users 0 members are here
  • 1 to 10
  • count
  • arduino
Related

HELP PLS

hadn05
hadn05 over 8 years ago

Well I want a variable to go like 1, 2, 3, 4, 5, 6, 7, 8, 9, 10 and then reset to 1 and then goes from 1 to 20. HOW DO I DO IT??

  • Sign in to reply
  • Cancel

Top Replies

  • koudelad
    koudelad over 8 years ago +3 suggested
    https://www.arduino.cc/reference/en/language/structure/control-structure/for/
  • 14rhb
    14rhb over 8 years ago in reply to scmclain +3 suggested
    I'm sure there are many E14 members who could write the exact code you are after, but I suggest a better way to understand it would be to try out the code in your own Arduino IDE - e.g. the code that scmclain…
  • scmclain
    scmclain over 8 years ago in reply to hadn05 +2 suggested
    Let me try to explain the example code from the link above. I am on my phone, so this may not work so well. Example Code // Dim an LED using a PWM pin int PWMpin = 10 ; // LED in series with 470 ohm resistor…
Parents
  • koudelad
    0 koudelad over 8 years ago

    https://www.arduino.cc/reference/en/language/structure/control-structure/for/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hadn05
    0 hadn05 over 8 years ago in reply to koudelad

    can you give me the code I don't really understand the for loop thingy @koudelad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scmclain
    0 scmclain over 8 years ago in reply to hadn05

    Let me try to explain the example code from the link above. I am on my phone, so this may not work so well.

     

    Example Code

     

    // Dim an LED using a PWM pin 
    int PWMpin = 10; // LED in series with 470 ohm resistor on pin 10 

    void setup()
    { // no setup needed } 
    void loop()
    { for (int i=0; i <= 255; i++)
    { analogWrite(PWMpin, i);
    delay(10); }
    }

     

    The line that has the “for” function declares variable “i” as an integer and sets the value to 0. The “for” loop will run as long as i is less than or equal to 255. It will send the value of i to the PWM pin to vary the brightness of the LED. the i++ means that the variable i gets incremented each loop.

     

    instead of writing the value of i to a pin, you could print it instead.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 8 years ago in reply to scmclain

    I'm sure there are many E14 members who could write the exact code you are after, but I suggest a better way to understand it would be to try out the code in your own Arduino IDE - e.g. the code that scmclain has kindly just explained. Then start to adjust that code and hopefully how it works will become clearer. If you get stuck then post the error messages and your existing code and we'll help you along image.

     

    If you understand what scmclain has explained then you may want to look up 'nested loops' to do your two separate counts (like this link at Tutorialspoint ).

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 8 years ago in reply to scmclain

    I'm sure there are many E14 members who could write the exact code you are after, but I suggest a better way to understand it would be to try out the code in your own Arduino IDE - e.g. the code that scmclain has kindly just explained. Then start to adjust that code and hopefully how it works will become clearer. If you get stuck then post the error messages and your existing code and we'll help you along image.

     

    If you understand what scmclain has explained then you may want to look up 'nested loops' to do your two separate counts (like this link at Tutorialspoint ).

     

    Rod

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer