Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum programmable frequency generator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 31 replies
  • Answers 18 answers
  • Subscribers 416 subscribers
  • Views 4320 views
  • Users 0 members are here
  • programmable function generator
Related

programmable frequency generator

blisk
blisk over 8 years ago

Can anyone help me with this.

I need programmable frequency generator which will work like described below.

 

Something I can setup like this

program 1) 20Khz sinus, 20 minutes -ON

program 2) 460Khz sinus, 25 minutes - ON

program 3) 20Hz sinus, 40 minutes - ON

program 4) 201Hz sinus, 20 minutes - OFF

program 5) 300Hz sinus, 20 minutes - OFF

program 6) 500KHz sinus, 40 minutes - OFF

program 7) 1,5Khz saw, 16 minutes - ON

program 8) 200Hz sinus, 40 minutes - OFF

program 9) 15Khz square, 16 minutes - ON

program 10) 25Khz square, 16 minutes - ON

program 11) 600Hz square, 10 minutes - ON

program 12) 100Khz saw, 5 minutes. - ON

 

Every program I can set some frequency and wave form and time how much time it will run and On or OFF for certain program. One program will run and when it ends goes to next one which is ON and skips one which is OFF until the last one with ON, after that goes to start and repeats again. But If I setup that all programs goes just one loop it will stop when last one ends

but If I setup it must take 10 or 20 loops it will goes from start to the end as many times I setup, If I setup infinity it will run whole time.

I hope it is possible to have at least three program loops (from program 1 to program 12) like this so I can choose which one to run, and hope I can set this over internet also, but it also needs to have a display where I can setup all of that if internet is not availible. Exit must go to some amplifier which give out about 10W.

 

I know this is a complicated project but can someone help me. Don't know what to use for this arduino or some Atmel or something else.

And nex I don't know nothing about programming so I will need some extra help here.

 

Something like this but with more functions like this.

[URL=www.ebay.com/.../111438305665 generator[/URL]

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +6 suggested
    I'm intrigued - what is this for ? (If you are able to tell). The range of frequencies is such that the DDS based approach is by far the simplest. The board Shabaz suggests looks fine. I've used the AD5984…
  • michaelkellett
    michaelkellett over 8 years ago in reply to shabaz +6 suggested
    Here's a really quick and dirty 10MHz audio amp: It's a rather evil circuit because: 1) several of the semis are operating at the max power they can stand with 10V pk-pk output 2) The output devices are…
  • shabaz
    shabaz over 8 years ago +5 suggested
    Hi Dennis, The frequency generation bit is really easy to do, but with a DDS board attached to your Arduino (or any other microcontroller). Something like this, can attach with just a few wires: https…
  • shabaz
    0 shabaz over 8 years ago

    Hi Dennis,

     

    The frequency generation bit is really easy to do, but with a DDS board attached to your Arduino (or any other microcontroller).

    Something like this, can attach with just a few wires:

    https://www.ebay.co.uk/itm/AD9834-Signal-Generator-Module-DDS-Signal-Source-Board-Sine-Triangle-Square-Wave/282729270172?hash=item41d3fa4b9c:g:0z0AAOSwi0xaBlA2

     

    A small bit of code is needed to configure it. I'm sure someone will have done it for Arduino already, and you could modify it to suit your requirements.

    I've used it but not with an Arduino.

    Modifying an existing program to suit your requirements is not difficult, but will involve you spending a couple of days doing Arduino tutorials to get familiar with its capabilities and how to write simple programs. Anyone can code for it, but does need a day or two of reading and practice.

    Otherwise, if this is a work project, then almost any function generator will work, if you check it has USB or Ethernet connection - then you can instrument all this from your PC to meet your requirements. Jan Cumps has a series on using LabView for example, which you can check by clicking on his name and then going to his content.

    The amplifier bit is not easy to do, you might get lucky and find something off-the-shelf but it may not be cheap. You're outside of the frequency range of most audio amps, otherwise that could have been an option..

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to shabaz

    yes, if you include SCPI functionality in your design, you can use the usual lab automation tools to control your instrument.

    You could use the PWM module of your microcontroller to generate square waves. Fairly simple opamp circuits can be used to derive sawtooth and sinus signals from that square wave.

     

    I have a full functional SCPI square wave generator here on element14, using a TI LaunchPad. You could start from there and add the analog parts to the output.

     

    Create a Programmable Instrument with SCPI - Part 1: Parser Library

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago

    I'm intrigued - what is this for ? (If you are able to tell).

     

    The range of frequencies is such that the DDS based approach is by far the simplest. The board Shabaz suggests looks fine. I've used the AD5984 and it isn't very hard to control.

     

    Rigol sell a 10W power amp which will work over the frequency range you need - I've never seen a cheaper one to buy than this (but I could make one much cheaper if I had to image)

     

    https://www.rigol-uk.co.uk/Rigol-PA1011-10W-Power-Amplifier-p/pa1011.htm

     

    You might still need a low power amplifier between the DDS board and the Rigol power amplifier.

     

    Do you have any funds for this project  or does it all have to be ultra cheap ?

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to michaelkellett

    michaelkellett  wrote:

     

    I'm intrigued - what is this for ? (If you are able to tell).

     

    ...

     

    Do you have any funds for this project  or does it all have to be ultra cheap ?

     

    MK

    If it is a one-off, using development boards for the microcontroller and the signal generator, and an off-the-shelf amplifier like the Rigol, I’d assess hardware costs to be somewhere around 500€.

     

    Because blisk doesn’t have program skills, someone would have to build the firmware (microcontroller talking to the AD chip and exposing an api that can be used to set the frequency and wave form).

    Someone (else) would also have to write the specific control program to drive the instrument to step through the particular set of steps that blisk needs.

    Building an API that’s as flexible as he wants it, and allows him to set up himself with no program skills, would require another level of abstraction so that it can be configured flexibly by a non-coder.

     

    If the person that makes that firmware, and the wrapper that allows blisk to flexibly configure it, asks a normal market price for the hours spent developing all of it, I assess a figure in the several 1000s of €.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blisk
    0 blisk over 8 years ago in reply to michaelkellett

    Yes it should be ultra cheap and it is not for something for selling but for healing purpose with frequency for me.

     

    I know that project is a bit difficult but I think it can be made step by step, that means upgrading it until I get what I want.

     

     

    500€ is alot for this project.

    I am here for help if that is not possible than it is not possible I will accept that.

    I thought with arduino that will not be that hard to do that.

     

    I have experiences with electronics but not with micro controllers.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to blisk

    If you have hardware skills, you can save a lot by making your own 10W amplifier. That one was more than 300 € so you can save on that. You can also save on the signal generator because for frequency therapy, precision and  noise aren't important. You would not need the coax connectors and converters.

     

    Is there a specific need in the healing functionality for sinus and sawtooth? If not, yoj'd only need the pwm of a microcontroller, and the 10W self-built amp.

     

     

    And the firmware could use an SD card to get the instructions. SD card readers are available for the arduino. You would create a text file on your computer and write it to the card.

    Then insert the card in the arduino and power on.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blisk
    0 blisk over 8 years ago in reply to Jan Cumps

    Yes sinus and sawtooth signals are important too. Amplifier I will make it by my own problem is because amplifier must amplify high frequencies.

    I can use SD card that is no problem.

    So what to use for start and it should have display?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to blisk

    according to your specs you don’t need a display.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blisk
    0 blisk over 8 years ago in reply to Jan Cumps

    But I do need display, I plan to use this withouth computer.

    Can I use this? I get this from a friend.

     

    https://www.robotics.org.za/W6705

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to blisk

    that’s an fpga. Way overkill for what you need, and the learning curve to build a design with it is significant.

    Your requirements don’t call for a display, even if run without Pc. you don’t need a button either.

    you need electronics that can generate sine, sawtooth and square, a programmable switch that can select one of those signals, and a broadband 10W amplifier.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>