Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Problem in POST data to Server
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 415 subscribers
  • Views 1220 views
  • Users 0 members are here
Related

Problem in POST data to Server

yashcool
yashcool over 8 years ago

I have to send data on server using SIM900A

but when I send data to server it just send BLANK DATA on server.

please suggest me what the mistake in code.

 

Thank you

 

Here Is my code:--------

 

#include<SoftwareSerial.h>

SoftwareSerial serial(2, 3);//rx, tx

 

void setup()

{

    serial.begin(9600);

    Serial.begin(9600);                   //Initialize a serial communication with baud rate 9600

    //delay(500); 

}

 

 

void loop()

{

      UploadData(aurdino); 

      delay(1000);

}

 

//Data uploading

void UploadData(String i)

{

      serial.println("AT+CGATT=1");

      delay(1000);

      toSerial();

      delay(2000);

 

      serial.println("AT+SAPBR=3,1,\"CONTYPE\",\"GPRS\"");

      delay(1000);

      toSerial();

      delay(3000);

     

      serial.println("AT+SAPBR=3,1,\"APN\",\"airtelgprs.com\"");

      delay(1000);

      toSerial();

      delay(3000);

     

      //Enable bearer 1

      serial.println("AT+SAPBR=1,1");

      delay(1000);

      toSerial();

      delay(3000);

 

     //Check whether bearer 1 is open.

     serial.println("AT+SAPBR=2,1");

     delay(1000);

     toSerial();

     delay(1000);

    

    //Initialize HTTP service

     serial.println("AT+HTTPINIT");

     delay(1000);

     toSerial();

     delay(3000);

 

      //Set the context ID

      serial.println("AT+HTTPPARA=\"CID\",1");

      delay(1000);

      toSerial();

      delay(3000);

   

     serial.println("AT+HTTPPARA=\"URL\",\"http://xxxxxxxxxxx/xxxxxx/insert.php?arduno=122");

                 

     //Set up the HTTP action  

     serial.println("AT+HTTPACTION=1");

     delay(1000);

     toSerial();

     delay(6000);

   

      //Do a HTTP read

     serial.println("AT+HTTPREAD");

     delay(1000);

     toSerial();

     delay(10000);

 

     //Terminate the HTTP service

     serial.println("AT+HTTPTERM");

     delay(1000);

     toSerial();

     delay(3000);

 

}

 

void toSerial()

{

  while(serial.available()>0)

  {

    Serial.write(serial.read());

  }

 

  delay(200);

}

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 8 years ago +1
    There are two parts to this solution. The sending part (i.e. the Arduino code), which you have provided, and the receiving part (i.e. the php code), which we will need to see.
  • yashcool
    yashcool over 8 years ago in reply to BigG +1
    i have php code Attachments: community.element14.com/.../incert.php.txt.zip community.element14.com/.../write.php.txt.zip
  • BigG
    0 BigG over 8 years ago

    There are two parts to this solution. The sending part (i.e. the Arduino code), which you have provided, and the receiving part (i.e. the php code), which we will need to see.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • yashcool
    0 yashcool over 8 years ago in reply to BigG

    i have php code

    Attachments:
    incert.php.txt.zip
    write.php.txt.zip