Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Location Tracking
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 9 answers
  • Subscribers 418 subscribers
  • Views 3660 views
  • Users 0 members are here
Related

Location Tracking

rgiguere
rgiguere over 8 years ago

Ok so we have all seen autonomous lawnmowers. I am currently building my own which is relatively easy to do the problem is location tracking.  I do not want to use a bunch of burried wire to create a path for it to follow and just setting up a perimeter makes it wander around aimlessly. GPS is not accurate enough to get propper location RF signals seem to be extremely complicated and relatively expensive so my question is is there any other way to track the location of a rover acuratley enough to be within 1 foot or less?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +4 suggested
    Hi Robert, Without local things to sense (like buried wires etc) I think it's not easy to do it repeatably with reliability, and that's of prime importance for your use-case I guess. If you have the ability…
  • Gough Lui
    Gough Lui over 8 years ago in reply to shabaz +3 suggested
    If not via a visual system, radio is a bit tricky to localise, but light generally is not. I wonder whether you could rig up some criss-crossed high-power infrared beams or something like that. Detect…
  • jw0752
    jw0752 over 8 years ago +3 suggested
    I have a robot vacuum cleaner that does a great job of mapping a room. It has several forms of obstacle detection but seems to have a way of counting its steps (wheel revs) and keeping track of its direction…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Robert,

     

    Without local things to sense (like buried wires etc) I think it's not easy to do it repeatably with reliability, and that's of prime importance for your use-case I guess.

    If you have the ability to mount a camera high up with visibility of the entire area (not at a shallow angle) then things could be easier, but would require something like a Pi.

    With that and the camera attachment plugged in, you can use software called 'OpenCV' to recognize the lawnmower and its co-ordinates.  It is quite effective, and easier still if there is some special color or large pattern on the lawnmower.

    Then some maths is needed to translate that into a real position and then translate that into instructions that would direct the lawnmower correctly. It's a lot of work to do though, it wouldn't be a quick solution.

    You could also check out ROS (Robotic Operating System) - that may have suitable plugins or apps for camera feeds (e.g. a camera attached to your device) and image processing, but again this is a lot of work if you've never used it before. That's not to say you shouldn't attempt it - lots of useful skills can be learnt by doing this, even if the end goal is still far away, and you may then be in a better position to decide if you wish to continue that path, or not.

    If you have the time and a Linux box (e.g. Pi) and some camera, it is quite straightforward to get going with OpenCV.

    To do that, go to https://www.raspberrypi.org/magpi/  and in the search box (unintuitively not at the top of the page, but below the banner) type opencv to find articles on image recognition type topics which is what the camera method approximately needs - I have not read them, but they are designed for beginners. You'll probably also want to get a book on the subject from your library or Amazon etc.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to shabaz

    If not via a visual system, radio is a bit tricky to localise, but light generally is not. I wonder whether you could rig up some criss-crossed high-power infrared beams or something like that. Detect obstruction by lawnmower to determine location. Or do a little more sophisticated like some of the laser-ranging devices and actually get a distance measurement as well? A bit hard in outdoor sunlight or inclement weather though.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 8 years ago in reply to shabaz

    If not via a visual system, radio is a bit tricky to localise, but light generally is not. I wonder whether you could rig up some criss-crossed high-power infrared beams or something like that. Detect obstruction by lawnmower to determine location. Or do a little more sophisticated like some of the laser-ranging devices and actually get a distance measurement as well? A bit hard in outdoor sunlight or inclement weather though.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer