Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum QUESTION
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 417 subscribers
  • Views 975 views
  • Users 0 members are here
Related

QUESTION

richipearl
richipearl over 8 years ago

please, is arduino a good start point for me and after arduino what's next, I need your advise I'm studying entrepreneurship study in school and I'm in my industrial training period due to my love for embedded system I choose to learn arduino.

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 8 years ago +6 suggested
    I like to think of Arduino as an ecosystem, with it's IDE and all the shields and libraries etc. rather than a single product. It has essentially become, in my opinion, the hardware version of a spreadsheet…
  • Fred27
    Fred27 over 8 years ago +5 suggested
    Although I'm personally not a fan of the whole Arduino thing, you will find it's an easy way to get started with embedded development and there's lots of information out there. For the same reason, the…
  • dougw
    dougw over 7 years ago +2
    I think the above suggestions are great. There are so many arduino examples available, it provides an easy learning path for most applications. I would also recommend Cypress PSoC Creator - it is generally…
Parents
  • BigG
    0 BigG over 8 years ago

    I like to think of Arduino as an ecosystem, with it's IDE and all the shields and libraries etc. rather than a single product.

     

    It has essentially become, in my opinion, the hardware version of a spreadsheet (which is software consisting of charting/visualisations, analytics, macros and data entry options).

     

    My reasoning is that when you want to carry out some initial analysis for a project, you are most likely to start with a spreadsheet to test out your analytical model, than go out and develop custom software to achieve the same purpose. This is especially true if you are doing the analysis for the first time and you are not familiar with what you are trying to achieve. Starting off with advanced analytics software or complex databases is more often than not, like taking a sledgehammer to crack a nut and you can quickly get delayed or hit problems due to lack of familiarity or community support.

     

    So while spreadsheet software might not have the performance and speed, it is certainly very versatile and you are able to use if for many different projects or assignments etc.

     

    However, if your spreadsheet model becomes more complicated or if you distribute your spreadsheet model to others, you will quickly hit problems. It is then that other types of software products becomes more useful and valuable to you, or you may even consider developing your own customised software.

     

    In my experience, the same can be said about Arduino.

     

    It is a very good starting point for evaluating a proof of concept, for example. I often find that it is the quickest way to verify that a new sensor you've just purchased actually works properly, simply because of the abundance of libraries available. Arduino is also very useful for reuse especially when looking to capture data for a specific task etc. Setup is quick and relatively easy.

     

    After Arduino, what's next?

     

    Well, much like moving on from a spreadsheet, your choice of options depends on the specific requirements of your project or intended product.

     

    From an entrepreneur's perspective, cost and speed to deliver an outcome are very important criteria. Also availability of resource to actually deliver the work. So you wouldn't necessarily pick something that only a select few know about, unless you have very specific reasons for that choice of hardware.

     

    ... and funnily enough this is where a spreadsheet model becomes very handy in helping you formulate that decision, as it will be based on multiple hard and soft criterion.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • BigG
    0 BigG over 8 years ago

    I like to think of Arduino as an ecosystem, with it's IDE and all the shields and libraries etc. rather than a single product.

     

    It has essentially become, in my opinion, the hardware version of a spreadsheet (which is software consisting of charting/visualisations, analytics, macros and data entry options).

     

    My reasoning is that when you want to carry out some initial analysis for a project, you are most likely to start with a spreadsheet to test out your analytical model, than go out and develop custom software to achieve the same purpose. This is especially true if you are doing the analysis for the first time and you are not familiar with what you are trying to achieve. Starting off with advanced analytics software or complex databases is more often than not, like taking a sledgehammer to crack a nut and you can quickly get delayed or hit problems due to lack of familiarity or community support.

     

    So while spreadsheet software might not have the performance and speed, it is certainly very versatile and you are able to use if for many different projects or assignments etc.

     

    However, if your spreadsheet model becomes more complicated or if you distribute your spreadsheet model to others, you will quickly hit problems. It is then that other types of software products becomes more useful and valuable to you, or you may even consider developing your own customised software.

     

    In my experience, the same can be said about Arduino.

     

    It is a very good starting point for evaluating a proof of concept, for example. I often find that it is the quickest way to verify that a new sensor you've just purchased actually works properly, simply because of the abundance of libraries available. Arduino is also very useful for reuse especially when looking to capture data for a specific task etc. Setup is quick and relatively easy.

     

    After Arduino, what's next?

     

    Well, much like moving on from a spreadsheet, your choice of options depends on the specific requirements of your project or intended product.

     

    From an entrepreneur's perspective, cost and speed to deliver an outcome are very important criteria. Also availability of resource to actually deliver the work. So you wouldn't necessarily pick something that only a select few know about, unless you have very specific reasons for that choice of hardware.

     

    ... and funnily enough this is where a spreadsheet model becomes very handy in helping you formulate that decision, as it will be based on multiple hard and soft criterion.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer