Arduino Forum Arduino beginner
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
  • Replies 5 replies
  • Subscribers 392 subscribers
  • Views 478 views
  • Users 0 members are here
Related

Arduino beginner

Former Member
Former Member over 10 years ago

I'm fairly new to using an arduino and i've been trying to get a project to display numbers to a 8x8 led matrix and i'm having trouble getting it to display. All i get is is just a flashing of random lights on the matrix or two columns just stay lit and no interaction between my arduino and the display seems to be happening. Any way someone could trouble shoot my code and see if its a code error?

 

Here is the code:

 

#include <LedControl.h>

#define Num0 {B00111100, B01111110, B01100110, B01100110, B01101100, B01101100, B01111110, B00111100}

#define Num1 {B00011000, B00111000, B00111000, B00011000, B00011000, B00011000, B01111110, B01111110}

#define Num2 {B01111100, B01111110, B00000110, B00111110, B01111100, B01100000, B01111110, B00111110}

#define Num3 {B01111100, B01111110, B00000110, B00011110, B00011110, B00000110, B01111110, B01111100}

#define Num4 {B01100110, B01100110, B01100110, B01111110, B01111110, B00000110, B00000110, B00000110}

#define Num5 {B00111110, B01111110, B01100000, B01111100, B00111110, B00000110, B01111110, B01111100}

#define Num6 {B01111110, B01111110, B01100000, B01111110, B01100010, B01100010, B01100010, B01111110}

#define Num7 {B01111110, B01111110, B00000110, B00000110, B00000110, B00000110, B00000110, B00000110}

#define Num8 {B00111100, B01100110, B01100110, B01111110, B01111110, B01100110, B01100110, B00111100}

#define Num9 {B00111100, B01111110, B01100110, B01111110, B00111110, B00000110, B00000110, B00000110}

LedControl lc=LedControl(12,11,10,1);

unsigned long delayTime=1000;

byte number1[] = Num1;

byte number2[] = Num2;

byte number3[] = Num3;

byte number4[] = Num4;

byte number5[] = Num5;

byte number6[] = Num6;

byte number7[] = Num7;

byte number8[] = Num8;

byte number9[] = Num9;

byte number0[] = Num0;

 

 

void setup()

  // put your setup code here, to run once:

{

  lc.shutdown(0,false);  // Wake up displays

  lc.shutdown(1,false);

  lc.setIntensity(0,5);  // Set intensity levels

  lc.setIntensity(1,5);

  lc.clearDisplay(0);  // Clear Displays

  lc.clearDisplay(1);

}

void snumber0()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number1[i]);

  }

}

 

 

  void snumber1()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number1[i]);

  }

}

 

 

  void snumber2()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number2[i]);

  }

}

  void snumber3()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number3[i]);

  }

}

  void snumber4()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number4[i]);

  }

}

  void snumber5()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number5[i]);

  }

}

  void snumber6()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number6[i]);

  }

}

  void snumber7()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number7[i]);

  }

}

  void snumber8()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number8[i]);

  }

}

  void snumber9()

{

  for (int i = 0; i< 8; i++)

  {

    lc . setRow(0,i,number9[i]);

  }

}

 

 

void loop() {

    snumber0();

    delay(delayTime);

    snumber1();

    delay(delayTime);

    snumber2();

    delay(delayTime);

    snumber3();

    delay(delayTime);

    snumber4();

    delay(delayTime);

    snumber5();

    delay(delayTime);

    snumber6();

    delay(delayTime);

    snumber7();

    delay(delayTime);

    snumber8();

    delay(delayTime);

    snumber9();

    delay(delayTime);

   

 

 

}

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    There seems to be nothing in particular wrong with your code but can you provide the library or a link to it

    and also a link to the hardware your using with a schematic please

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    here is the link to where i got the library: https://brainy-bits.com/tutorials/how-to-control-max7219-led-matrix/

    Here is the link for a schematic of my hardware: http://playground.arduino.cc/Main/MAX72XXHardware#Wiring

    Now what i was trying to do was follow brainy-bits to get it up and making sure my numbers displayed correctly then change the code so when i push a button the numbers change and hopefully get it to act as a score counter. I don't know if that helps at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    here is the link to where i got the library: https://brainy-bits.com/tutorials/how-to-control-max7219-led-matrix/

    Here is the link for a schematic of my hardware: http://playground.arduino.cc/Main/MAX72XXHardware#Wiring

    Now what i was trying to do was follow brainy-bits to get it up and making sure my numbers displayed correctly then change the code so when i push a button the numbers change and hopefully get it to act as a score counter. I don't know if that helps at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 10 years ago in reply to Former Member

    Does the code from the link work as is? this would provide hardware is correctly valid and we can look at software. Otherwise the hardware is not right.

    C