Arduino Forum Robot Following The Person
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
  • Replies 12 replies
  • Subscribers 393 subscribers
  • Views 961 views
  • Users 0 members are here
Related

Robot Following The Person

Former Member
Former Member over 10 years ago

Hi,

I am working on a project, i.e following of a person by a robot.

 

I am not an expert although know enough to start with.

 

Please give me suggestions about the sensors so that i could use , which will help the robot to follow the person, also with suggestions please tell me a little how to use them.

 

NOTE: the robot should follow the specific person only if there are others.

 

PLEASE HELP!!

 

THANKs

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 10 years ago +4
  • fvan
    fvan over 10 years ago +2
    Have you seen this Ben Heck episode? Episode 38: See Ben Build an Autonomous Robot Luggage! He builds a suitcase that can follow him around, using ultrasonic sensors. Frederick
  • martinvalencia
    martinvalencia over 10 years ago +1
    You could use a webcam to recognize colors, such pre program the color polo that person use in this moment!
  • fvan
    fvan over 10 years ago

    Have you seen this Ben Heck episode? Episode 38: See Ben Build an Autonomous Robot Luggage!

     

    He builds a suitcase that can follow him around, using ultrasonic sensors.

     

    Frederick

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • martinvalencia
    martinvalencia over 10 years ago

    You could use a webcam to recognize colors, such pre program the color polo that person use in this moment!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to Workshopshed

    The simplest solution are always better image

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • martinvalencia
    martinvalencia over 10 years ago in reply to Workshopshed

    hehehe, the idea seems simple and very good!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    Maybe a dumb question, but can the person carry a device (transponder or something) that the robot can use as a vector input?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to Former Member

    I was thinking along the same lines too but was not sure if sensors would be sensitive enough on a small robot. In principle it's a case of looking at the difference in timing for the signal to arrive at different sensors. A bit like a quadrature encoder.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Workshopshed

    good idea

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    yeh why not , but if it is a device in small package

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago

    As Andy said, something like a quad encoder could control the vector.

     

    If you're thinking of fairly short distances something like the antenna-on-chip XBee's are great in a low-power small package.  I'd likely make the vector sensing a two-part system:

    1. Linked XBee's to let the robot know that it's paired device wants to be followed.  You could also use Bluetooth Low-Energy, I suppose.  I just prefer XBee, as you can get them in a 900MHz frequency band to avoid all the noise on the 2.4GHz ISM band.

    2. Ultrasound distance sensors to keep the robot at whatever distance you define from the person, but linked.  If the signal was blocked or became out of range you could code for some type of watchdog on the master to let the person know there was a problem.

     

    I know others prefer to use signal timing on a radio beam to let the slave know a vector.  That's an option also.  I'd put the onus on the user to be responsible for obstacle avoidance, and negotiating things like escalators.  On the other hand, if you like calculating Eigenvalues for autonomous robots, you could go that route. image

    It partly depends upon what type of control (and controller) you want to use.  If you want something that simply follows a master that's far less work than having a completely autonomous system.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>