Arduino Forum Anybody interested in our new ARM Cortex SAMD21J18 Arduino compatible board: The Autonomo?
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
  • Replies 3 replies
  • Subscribers 403 subscribers
  • Views 631 views
  • Users 0 members are here
  • autonomo
  • sodaq
  • arduino
Related

Anybody interested in our new ARM Cortex SAMD21J18 Arduino compatible board: The Autonomo?

janwillem
janwillem over 10 years ago

Hi Everyone,

 

The Arduino Uno has been on the marked for 10 years, so is a bit dated by now. We feel that the Future of Arduino is in ARM Cortex based boards.

It took Arduino over a year from first announcement to entering the market with the Arduino Zero (AKA Arduino M0 Pro and M0) but it is finally available now.

 

We have launched one of the first Arduino Zero compatible boards on Kickstarter:

 

https://www.kickstarter.com/projects/sodaq/autonomo-the-solar-powered-thing

 

Why the Autonomo? Well it is specifically built for the Internet of Things. In sleep it draws less than 30uA. It has serial flash and an SD card on board for data logging.

You can use a wide array of different 'bee' style communication modules with it (Xbee, GPRSbee, etc.) and it has a solar charge controller so it can run on a tiny solar panel:

 

Here it is next to the Arduino M0.

 

image

 

Thanks for your attention and welcome to our Kickstarter page.

 

The SODAQ Team

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 10 years ago in reply to bphilpot3 +1
    First, I don't know 100% for this particular board, but you can invoke the arduino command from the command line to build a sketch (note: you need version 1.5+). https://github.com/arduino/Arduino/blob…
  • bphilpot3
    bphilpot3 over 10 years ago

    Is it possible to develop for this board on a Linux host without the Arduino IDE?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to bphilpot3

    First, I don't know 100% for this particular board, but you can invoke the arduino command from the command line to build a sketch (note: you need version 1.5+).

     

    https://github.com/arduino/Arduino/blob/ide-1.5.x/build/shared/manpage.adoc

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • diablero
    diablero over 10 years ago

    Well, I'll make a visit on the site.