Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Help! Speech Recognition (upload error)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 415 subscribers
  • Views 1593 views
  • Users 0 members are here
  • help
Related

Help! Speech Recognition (upload error)

the_future
the_future over 7 years ago

Hi thanks for giving this a look at!

Was following a tutorial on youtube on Speech Recognition (geeetech module) as you (https://www.youtube.com/watch?v=Ur1tzMDP97g )

and I noticed that when I tried to upload the code I got a busy board and a runtime error whatever

that means.

 

What is funny is that I had to move to another computer to be able to upload any other code

to the boards but when I reuploaded the code on a new computer it gave me the same error again and stops me

from uploading any different code even a blank sketch.

 

Please help

Code:

 

byte com = 0;

 

void setup() {

     Serial.begin(9600);

 

     Serial.write(0xAA);

     Serial.write(0x37);

     delay(1000);

     Serial.write(0xAA);

     Serial.write(0x21);

}

 

void loop() {

 

  while(Serial.available()) {

       com = Serial.read();

       switch(com) {

 

      case 0x11:   //command 1

      Serial.println("a");

      break;

 

      case 0x12:  //command 2

      Serial.println("b");

      break;

 

 

      case 0x13:  //command 3

      Serial.println("c");

      break;

 

 

      case 0x14:  //command 4

      Serial.println("d");

      break;

 

 

      case 0x15:  //command 5

      Serial.println("e");

      break;

 

            }

      }

}

 

 

 

 

Mega Error Messages:

 

"Arduino: 1.8.5 (Windows 10), Board: "Arduino/Genuino Mega or Mega 2560, ATmega2560 (Mega 2560)" Genuino Mega or Mega 2560, ATmega2560 (Mega 2560)"

Sketch uses 2084 bytes (0%) of program storage space. Maximum is 253952 bytes.

Global variables use 199 bytes (2%) of dynamic memory, leaving 7993 bytes for local variables.Maximum is 8192 bytes.

 

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_ReceiveMessage(): timeout

avrdude: stk500v2_getsync(): timeout communicating with programmer An error occurred while uploading the sketch

 

 

 

 

Uno Error Messages:

 

Arduino: 1.8.5 (Windows 10), Board: "Arduino/Genuino Uno"

Sketch uses 1786 bytes (5%) of program storage space. Maximum is 32256 bytes.

Global variables use 199 bytes (9%) of dynamic memory, leaving 1849 bytes for local variables.Maximum is 2048 bytes.

 

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 1 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 2 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 3 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 4 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 5 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 6 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 7 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 8 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 9 of 10: not in sync: resp=0x68

avrdude: stk500_recv(): programmer is not responding

avrdude: stk500_getsync() attempt 10 of 10: not in sync: resp=0x68

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +3 suggested
    Check you have selected the correct board type and serial port. It looks like the Arduino IDE is having problems communicating with the microcontroller on the board. My suspicion is that you may have a…
  • Gough Lui
    Gough Lui over 7 years ago in reply to the_future +2 suggested
    The way you've wired or designed your sketch is probably not the best for an Arduino Uno which has a single UART port. You're trying to use the UART to communicate with the module itself, and it seems…
  • shabaz
    shabaz over 7 years ago +1 suggested
    Hi, It looks like a driver, program installation, software version, or connection issue. I don't have any more knowledge in this area though. From the error message, it is unlikely to be anything to do…
Parents
  • Gough Lui
    0 Gough Lui over 7 years ago

    Check you have selected the correct board type and serial port. It looks like the Arduino IDE is having problems communicating with the microcontroller on the board. My suspicion is that you may have a shield or some other circuitry that is using the Pin 0 or Pin 1 on the Arduno Uno (i.e. its UART port pins) or attempting to communicate with the board during programming corrupting the data. As a result, communication is not being established with the ATMega microcontroller and the programmer times out.

     

    Try removing any shields or anything connected to the Arduno Uno board and try programming again. Once programmed, then reattach the shield to see if it works. Some shields have switchable serial lines so you can use other pins with SoftwareSerial or you can temporarily disconnect the UART connection to prevent interfering with sketch upload.

     

    If this doesn't help and nothing is attached to Pin D0/D1 ... you may have something else going on - e.g. a damaged bootloader on the ATMega microcontroller which you might need to use ArduinoISP and another working Arduino to recover from.

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the_future
    0 the_future over 7 years ago in reply to Gough Lui

    Hi thanks for this great help it now uploads when I remove the pins of the Geeetech Voice Module attached to the TX (pin 1) and RX (pin 0) of the Arduino Uno board, however even though it uploads when I say the words I have stored and imported to the module in "Group 1" nothing happens. See tutorial I am following -> https://youtu.be/Ur1tzMDP97g

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • the_future
    0 the_future over 7 years ago in reply to Gough Lui

    Hi thanks for this great help it now uploads when I remove the pins of the Geeetech Voice Module attached to the TX (pin 1) and RX (pin 0) of the Arduino Uno board, however even though it uploads when I say the words I have stored and imported to the module in "Group 1" nothing happens. See tutorial I am following -> https://youtu.be/Ur1tzMDP97g

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to the_future

    The way you've wired or designed your sketch is probably not the best for an Arduino Uno which has a single UART port. You're trying to use the UART to communicate with the module itself, and it seems you're trying to read a response from the module and communicate with the computer. While it could possibly work, I'm not sure it's necessarily a great idea to do it this way as most UARTs are designed to "talk" to one partner only and if there is a disagreement between the logic levels (e.g. module sends a high but the USB-Serial bridge sends a low) then you're likely to cause a short which would either stress or damage the UART. For a Uno, it's probably best to have the module hosted on its own separate SoftwareSerial instance which can run on its own pins separate from the 0/1 which are used for communication with the PC via the USB-Serial bridge.

     

    With different boards (e.g. the Arduino Leonardo ATMega32u4-based boards), the UART pins (0/1) are separate from the serial monitor console (emulated USB serial port) which would allow this sort of configuration to work but in return they come with their own complications to do with port enumeration on resetting which can cause its own headaches.

     

    Regardless, at this point, you may have uploaded the sketch correctly, but if nothing happens then it seems several possibilities could be the cause:

    • The module itself may not be sending the response you are expecting - maybe it's not functioning, not correctly powered, not receiving the input it expects.
    • The Arduino may not be receiving the response from the module it expects and is not generating the output you expect - perhaps you have RX/TX swapped or there is something subtle wrong with the code such as a baud rate mismatch between the module and Arduino or more likely, there's a logic level clash because you have multiple drivers connected to an input as I mentioned earlier.
    • The PC may not be receiving the expected response from the Arduino - this may be because the terminal emulator baud rate is incorrectly set, because of incorrect port selection or for some other reason.

     

    You really need to break the problem down to identify where the issue is. Perhaps if you have access to an oscilloscope, start by seeing what is happening on the data lines and whether it corresponds to what you're expecting (e.g. response from module).

     

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer