Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino Bluetooth send data to Python stuck
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 414 subscribers
  • Views 2408 views
  • Users 0 members are here
Related

Arduino Bluetooth send data to Python stuck

i7-ryzen
i7-ryzen over 7 years ago

Hi, I have spent almost 3 days scouting the web for this solution but to not available.

 

I have an Arduino UNO R3 + bluetooth HC-05 and want to transmit information through Bluetooth to Laptop Win10 + Python Pybluez.

 

It appears that the only information I can receive using revc in Python are those send through Serial monitor and not Bluetooth. EVEN WHEN THE ARDUINO IS NOT PHYSICALLY CONNECTED TO THE COMPUTER (only through bluetooth), revc still only returns the values printed to Serial.

 

Arduino code

#include <SoftwareSerial.h>

//Define the pins used for receiving
//and transmitting information via Bluetooth
const int rxpin = 0;
const int txpin = 1;

//Variable to store input value
char rec= 'A';

//Connect the Bluetooth module
SoftwareSerial bluetooth(rxpin, txpin);

void setup(){
  //Initialize Serial for debugging purposes
  Serial.begin(9600);
  Serial.println("Serial ready");
  //Initialize the bluetooth
  bluetooth.begin(9600);
  bluetooth.println("Bluetooth ready");
}

void loop(){
  if(bluetooth.available()){
    rec = bluetooth.read(); // read 1 char
    Serial.println(rec);    // Printout throught Serial the Char just read.
  }   
  if(rec == 'Z'){ // If rec char is Z          
    Serial.println("Serial: Z"); // Printout throught Serial
    bluetooth.println("Bluetooth: Z"); // Printout throught Bluetooth
    rec = 'A'; // reset rec to A to avoid inf loop
  }
  //Wait ten milliseconds to decrease unnecessary hardware strain
   delay(10);
}

 

Python Codedevices = bluetooth.discover_devices()

 

import bluetooth

#Detect all Bluetooth devices and Create an array with all the MAC addresses
print("Searching for devices...")
nearby_
#Run through all the devices found and list their name
num = 0
print("Select your device by entering its coresponding number...")
for i in nearby_devices:
num+=1
print(str(num) + ": " + bluetooth.lookup_name( i ))
   
#Allow the user to select their Arduino
selection = int(input("> ")) - 1
bd_addr = nearby_devices[selection]
port = 1

# Show user selection
print("You have selected " + bluetooth.lookup_name(nearby_devices[selection]))

# Connect to bluetooth address and port
sock = bluetooth.BluetoothSocket( bluetooth.RFCOMM )
sock.connect((bd_addr, port))

data = "L"
sock.send(data)

data = "Z"
sock.send(data)

data = sock.recv(1024)
print(data)
# Print out appearsto be those of Serial.println and not bluetooth.println
   
sock.getsockname()
sock.getpeername()

sock.close()

 

Basically, I want only the data transmitted through "bluetooth.println".

 

The code above returns the following in Python:

 

b'L\r\nZ\r\nSerial: Z\r\n'

 

Expected return to be:

 

Bluetooth: Z\r\n

 

Thanks

 

Message was edited by: Formatted code.

  • Sign in to reply
  • Cancel
  • neilk
    0 neilk over 7 years ago

    Hi,

    You have defined, for use with SoftwareSerial

    1. constint rxpin = 0; 
    2. constint txpin = 1;

     

    These are actually the pins already used by the built in hardware serial port. That's why you are seeing the Serial Monitor Output on Bluetooth!

     

    If you want to communicate with your HC05 independently of the Serial Monitor, you must specify 2 different pins.for use with SoftwareSerial, and connect your HC05 to those pins.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer