Arduino Forum Sending multiple data from AppInventor to Arduino?
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
  • State Suggested Answer
  • Replies 10 replies
  • Answers 9 answers
  • Subscribers 401 subscribers
  • Views 2857 views
  • Users 0 members are here
  • arduino
Related

Sending multiple data from AppInventor to Arduino?

bopele
bopele over 6 years ago

I have 2 LEDs. With Slider1, I will adjust the brightness of one, Slider2 and the other. When I press these buttons in Animation 1 or Animation 2, the LEDs will light up in various ways. I have received data from Slider1 and Slider2, but how do I make changes to the AppInventor and Arduino code to receive and use the button data?

imageimage

image

  • Sign in to reply
  • Cancel

Top Replies

  • BigG
    BigG over 6 years ago +2 suggested
    Have you thought about what Arduino is receiving exactly. Remember, Arduino has no idea how you have designed the app. It just receives data from the Bluetooth Connection. So how are you telling Arduino…
  • BigG
    BigG over 6 years ago in reply to bopele +2 suggested
    It is pretty easy. As you are sending text via the"call BluetoothClient1.SendText" option, just prefix what you have in the "Join" with something you can parse out on the Arduino side. For Example, for…
  • neilk
    neilk over 6 years ago +1 suggested
    Hi bopele ane welcome to element14 It would help if you can explain what you actually want to do when the button(s) are pressed. Neil
Parents
  • BigG
    0 BigG over 6 years ago

    Yes as Neil indicated what you originally had works as you rely on the order to be consistent. blueSlider first, then orangeSlider. This becomes tricky when wanting to include button presses.

     

    I don't want to solve this for you, but could think about adding to this logic... which is to place or send the Button presses every time too but always before blueSlider and orangeSlider then you can infer that if these button values are zero then buttons were not pressed and therefore the next two values will be blueSlider and orangeSlider etc. Not saying this is the best way but just another option to think about.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • BigG
    0 BigG over 6 years ago

    Yes as Neil indicated what you originally had works as you rely on the order to be consistent. blueSlider first, then orangeSlider. This becomes tricky when wanting to include button presses.

     

    I don't want to solve this for you, but could think about adding to this logic... which is to place or send the Button presses every time too but always before blueSlider and orangeSlider then you can infer that if these button values are zero then buttons were not pressed and therefore the next two values will be blueSlider and orangeSlider etc. Not saying this is the best way but just another option to think about.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer