Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Creating DuPont equivalent crimp terminal
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 12 answers
  • Subscribers 413 subscribers
  • Views 6656 views
  • Users 0 members are here
Related

Creating DuPont equivalent crimp terminal

Andrew J
Andrew J over 7 years ago

What’s the generic term for the single pin crimp terminal to stick on the end of a wire in order to push into an Arduino header socket?  I’m used to the term Dupont connector but this isn’t a search term recognised by Farnell or CPC and there seems to be a fair mix of crimp terminals that may or may not be correct.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +8 suggested
    They are crimp sockets in rectangular housings but there are many terms used by different manufacturers and distributors. Consequently they are difficult to find, even though they are very common and almost…
  • fmilburn
    fmilburn over 7 years ago +8 suggested
    I have recently started crimping my own and have some Amphenol as well as inexpensive Chinese pins and sockets. I have the crimper that Shabaz linked above and like it. The Amphenol work well. The Chinese…
  • shabaz
    shabaz over 7 years ago +7 suggested
    Hi Andrew, I think it's just called a crimp socket, or a 0.1" SIL socket crimp terminal. Anyway, a typical one is this crimp socket crimp socket , it fits the 0.1" SIL pin headers on the Arduino. There…
Parents
  • shabaz
    0 shabaz over 7 years ago

    I had the camera out, so figured I'd take some photos.. I don't have the China crimps (although I did try them at one point) so cannot show the difference.

     

    Step 1: strip cable, by about 4mm (eyeballed, no real need to measure with the pin crimp, since there is space for the excess length. The socket crimps need a bit more accuracy but can still be eyeballed). I'm using thin wire (10/0.1, i.e. 10 strands of 0.1mm) so I like to fold it back, so I strip twice this amount.

    image

     

    Step 2:

    Since I'm using thin wire, I fold it back. Ignore this step if you get good results without doing this with your wire type.

    I just use a fingernail to fold it over, no need for pliers.

    image

     

    Step 3: Insert crimp so that the to-be-crimped portion of the crimp pin is flush with the tool crimping area. Then lightly press the tool (or ratchet by one step) so that the crimp pin is held in place and won't fall out. That will leave a free hand for the next step.

    image

    Step 4: Poke in the wire from the other side, so that you can just see it egressing from that tool crimping area.

    I should have taken the photo from the other side really. But the point is that the tip of the wire should be just visible coming out of the tool crimp area.

    Press the tool entirely until the ratchet releases.

    image

     

    Final result: (Normally I'll put some heatshrink sleeving over it).

    image

     

     

    Some other views of the crimped result:

    Some tool marks are visible, but this is heavily zoomed in, the actual amount of tool marks is acceptable I think.

    image

     

    The insulation clamping portion is visible here. I see no movement in that area when I bend the insulation to the right of the photo. It grips it well for this small diameter.

    image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Very useful pics, thanks Shabaz.  I figured out how the crimp tool works with Molex KK series terminals after a lot of head-scratching.  I suspect I may have the wire pushed too far forward, what do you think?  The wire itself is right on the border for size for that connector, but I've got some smaller gauge on order.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    I've not used these before, but your insulation area looks good (it should terminate near the red line marking below), the wire portion should terminate at the yellow line portion though it seems (I could be wrong).

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    I've not used these before, but your insulation area looks good (it should terminate near the red line marking below), the wire portion should terminate at the yellow line portion though it seems (I could be wrong).

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    I think you're right looking at it that close up.  The spring at the end is meant to depress when the pin is pushed into the receptacle, and it won't be able to with the wires there.

     

    I've ordered some thinner wire and more connectors, as well as the pin connectors you mentioned.  It's not surprising that I don't know what I actually need until I find myself thinking it's all well and good but how am I going to connect this to that.  Fortunately, I'm busy again this week so can't really get back to my project until Thursday.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer