Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino and wireless Rosemount 1410 gateway
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 7 answers
  • Subscribers 416 subscribers
  • Views 2290 views
  • Users 0 members are here
Related

Arduino and wireless Rosemount 1410 gateway

Sean_Miller
Sean_Miller over 7 years ago

Anyone have experience with having an Arduino talk to rosemount transmitters through the Rosemount 1410 gateways?

 

Im looking for a lead on code to make a call from the Arduino to a transmitter.

 

thanks,

sean

  • Sign in to reply
  • Cancel

Top Replies

  • Sean_Miller
    Sean_Miller over 7 years ago in reply to Sean_Miller +2
    Found the problem with the Rosemount 1410 not having the TCP/IP port open for Modbus. The vendor did not enable the feature on the 1410. I just need to enable the feature - or if it doesn't have the feature…
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to gam3t3ch +2 suggested
    Well, it worked! Using a python script with the pyModbusTCP library, it read in the registers. It took some detective work to find the address IDs to send. I also learned how Rosemount passes numbers through…
  • Sean_Miller
    Sean_Miller over 7 years ago +2 suggested
    Since there is a remote monitoring project14 running in this arena, I took the evening to better document this experience: Big Petro Maker Magic: $100 Datalogger That Can Save Millions Thanks for all your…
  • Sean_Miller
    0 Sean_Miller over 7 years ago in reply to gam3t3ch

    Well, it worked!  Using a python script with the pyModbusTCP library, it read in the registers.  It took some detective work to find the address IDs to send.

     

    I also learned how Rosemount passes numbers through the Modbus protocol.  It uses IEEE 754 floats which are represented by a 32 bits.  Two 16 bit registers are polled which return a decimal value to the python script.

     

    You have to move the last one in front of the first and then convert each to binary.  To get it from binary to the actual value, you have to solve a series of riddles such as bit one represents if it is a positive or negative number.  It's crazy, but allows for super accuracy of the data.  In the end, my script was 90% converting the two register values to an actual single float!

     

    Here's a reference of the IEEE 754 format:  https://www.h-schmidt.net/FloatConverter/IEEE754.html .

     

    See ya,

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 7 years ago

    Since there is a remote monitoring project14 running in this arena, I took the evening to better document this experience:

     

    Big Petro Maker Magic:  $100 Datalogger That Can Save Millions

     

    Thanks for all your input!

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<