Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Noob questions: Arduino Wi-Fi thermometer?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 417 subscribers
  • Views 1404 views
  • Users 0 members are here
Related

Noob questions: Arduino Wi-Fi thermometer?

sammybeany
sammybeany over 7 years ago

Apologies if this is in the wrong spot, I had some trouble navigating around the element14 site.

 

TL;DR summary: I need a simple way to get temperature and humidity readings into a PHP script. I want it to be powered by USB, but I want the data to be transferred over wi-fi. Where should I start?

 

Full story:

I have a tidy little PHP website I've made that pulls data from my Nest Thermostat via the unofficial API and generates this glanceable graph to show the current comfort level in my living room:

 

image

 

This is useful to me and I'm happy with it, but I want to enhance it with temperature and humidity readings from my second floor and my basement.

 

Nest makes their own external sensors, but they inexplicably lack a humidity reading. They're also battery powered, which I don't like, and they cost $40 each. I feel like I'd be better off trying to roll my own solution here.

 

I have extra USB charging outlets in the spots where I'd like to stash these sensors, so I figure that's the best way to power them.

 

I came across this tutorial, which seems quite close to what I'm looking for: https://www.instructables.com/id/Arduino-IOT-Temperature-and-Humidity-With-ESP8266-/

 

This guide seems to be a few years old, though, and I'm too much of a novice to know if there are ways to simplify and improve it. For one, I don't need data logging, I just need the sensor readings to be available on demand.

 

Any suggestions or ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 7 years ago +6 suggested
    ntewinkel kindly gave me access to his code and scripts as a starting point for my development of 2 channel ESP8266 based temperature monitoring system, with data sent over wifi to my own server. It's…
  • mp2100
    mp2100 over 7 years ago +5 suggested
    A quick look at that instructables makes me think that method is ok, and not too archaic. The funny thing is, those instructions areusing the esp8266 to add wifi to the arduino. If you really want to use…
  • ntewinkel
    ntewinkel over 7 years ago in reply to mp2100 +5 verified
    mp2100 wrote: ...the esp8266 is smart enough on its own... True, I've used some inexpensive ESP based boards to log data around the house here too. My favourite right now is still the Wemos D1 Mini. It…
Parents
  • luislabmo
    0 luislabmo over 7 years ago

    Hi Carl,

     

    I'd say there are many ways to do what you want. PHP is mainly for web development so I'd say is better to let another program -more up to the task- to handle the sensor reading like phyton; it would be probably easier to do and documentation for this is widely available.

    • On the webserver side you need two things:
      • Build a python script that reads the sensor data, and formats the output: it may be a text file, it may return a string, a number, etc., or the best one -I think- is to return the sensor readings in JSON format, like:

        import json
        print "Content-type: application/json"
        print 
        response={'Humidity':54}
        print(json.JSONEncoder().encode(response))

      • From the PHP script invoke such python script to read the data, something like:

        <?php 
        $command = escapeshellcmd('...dir..../readsensor.py');
        $output = shell_exec($command);
        ?>

     

    As others said, the ESP8266 is perfectly capable of reading the sensor and handling WiFi communication by itself, it just requires a little bit of coding but you don't need an extra Arduino to do the work (unless you don't want to tap into the ESP8266 code).

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 7 years ago

    Hi Carl,

     

    I'd say there are many ways to do what you want. PHP is mainly for web development so I'd say is better to let another program -more up to the task- to handle the sensor reading like phyton; it would be probably easier to do and documentation for this is widely available.

    • On the webserver side you need two things:
      • Build a python script that reads the sensor data, and formats the output: it may be a text file, it may return a string, a number, etc., or the best one -I think- is to return the sensor readings in JSON format, like:

        import json
        print "Content-type: application/json"
        print 
        response={'Humidity':54}
        print(json.JSONEncoder().encode(response))

      • From the PHP script invoke such python script to read the data, something like:

        <?php 
        $command = escapeshellcmd('...dir..../readsensor.py');
        $output = shell_exec($command);
        ?>

     

    As others said, the ESP8266 is perfectly capable of reading the sensor and handling WiFi communication by itself, it just requires a little bit of coding but you don't need an extra Arduino to do the work (unless you don't want to tap into the ESP8266 code).

     

    Luis

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer