Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Smart Control of Power Flow
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 8 answers
  • Subscribers 416 subscribers
  • Views 3366 views
  • Users 0 members are here
  • arduino-ide
  • arduino
Related

Smart Control of Power Flow

sayed94
sayed94 over 6 years ago

Hello guys, currently I am doing a project based on Power Sharing between Solar Home Systems by Smart Control of Power Flow. Any access energy will be share a common DC grid line (neighbouring PV system interconnected each other) based on a certain logic. I need to use a microcontroller which helps to control the power flow by certain simple logic below :

 

For a PV system, Initially, a microcontroller is checked the panel voltage, If panel voltage is available, then the solar panel will supply the load power. Also, the battery condition is checked simultaneously. If the state of charge of the battery is less than 90%, then the battery is also charged from panel voltage, otherwise, the excess panel voltage goes to the grid for sharing. In the meantime, If there is no panel voltage like abnormal weather and night times, the battery condition is checked and if there is significant charge in the battery, then battery supplies load with necessary voltage, else the microcontroller looks for available power from the grid to borrow where other SHS also interconnected. So voltage and the current sensor also included measuring the power how much send to the grid and how much (KWH or unit) take from the grid.

 

So now I need help, hopefully, someone will help me how can I start to code it in Arduino ....... or how can I model it MATLAB Simulink. I am looking forward to hearing someone

best regards
Thank You
Md Abu Sayed



  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +3 suggested
    Hi MD, I do not know the answer to your question but when I have been faced with similar problems in the past I have always started with a Logic Flow Chart. The next issue will be how you intend to sense…
  • shabaz
    shabaz over 6 years ago +3 suggested
    Hi MD, That's the approach I would use too, i.e. draw a flow chart or any description that completely defines the procedure (i.e. it becomes an algorithm of some sort), in your case maybe with inputs and…
  • fmilburn
    fmilburn over 6 years ago in reply to sayed94 +3 verified
    OK, that is helpful. I am glad to see from a safety viewpoint the voltage we are talking about is ~12V. This is not to dissuade you, but understand that what you are undertaking may be challenging. For…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi MD,

     

    That's the approach I would use too, i.e. draw a flow chart or any description that completely defines the procedure (i.e. it becomes an algorithm of some sort), in your case maybe with inputs and outputs that you wish your Arduino to sense and control. Then translate from your flow chart into pseudo-code. And then write the code from that.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sayed94
    0 sayed94 over 6 years ago in reply to shabaz

    I appreciate ur help
    by the way i did my algorithm but stack in converting algorithm into coding in arduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 6 years ago in reply to sayed94

    Hi,

    If you can attach a flow chart with inputs and outputs, even hand drawn, as suggested above it will help. Once that is done post the parts you are having trouble coding. Do you have any code or pseudo-code written at all?  It isn’t possible to help you in a meaningful way without more information.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sayed94
    0 sayed94 over 6 years ago in reply to fmilburn

    Hello @Sir
    this my complete information about my project including algorithm and pseudocode

    My project-based on Power Sharing between Solar Home Systems by Smart Control of Power Flow. Any access energy will be share a common DC grid line (neighbouring PV system interconnected each other) based on a certain logic. I need to use a microcontroller which helps to control the power flow by certain simple logic below :

     

    For a PV system, Initially, a microcontroller is checked the panel voltage, If panel voltage is available, then the solar panel will supply the load power. Also, the battery condition is checked simultaneously. If the state of charge of the battery is less than 90%, then the battery is also charged from panel voltage, otherwise, the excess panel voltage goes to the grid for sharing. In the meantime, If there is no panel voltage like abnormal weather and night times, the battery condition is checked and if there is significant charge in the battery, then battery supplies load with necessary voltage, else the microcontroller looks for available power from the grid to borrow where other SHS also interconnected. So voltage and the current sensor also included measuring the power how much send to the grid and how much (KWH or unit) take from the grid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sayed94
    0 sayed94 over 6 years ago in reply to fmilburn

    Hello @Sir
    this my complete information about my project including algorithm and pseudocode

    My project-based on Power Sharing between Solar Home Systems by Smart Control of Power Flow. Any access energy will be share a common DC grid line (neighbouring PV system interconnected each other) based on a certain logic. I need to use a microcontroller which helps to control the power flow by certain simple logic below :

     

    For a PV system, Initially, a microcontroller is checked the panel voltage, If panel voltage is available, then the solar panel will supply the load power. Also, the battery condition is checked simultaneously. If the state of charge of the battery is less than 90%, then the battery is also charged from panel voltage, otherwise, the excess panel voltage goes to the grid for sharing. In the meantime, If there is no panel voltage like abnormal weather and night times, the battery condition is checked and if there is significant charge in the battery, then battery supplies load with necessary voltage, else the microcontroller looks for available power from the grid to borrow where other SHS also interconnected. So voltage and the current sensor also included measuring the power how much send to the grid and how much (KWH or unit) take from the grid.