Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Turning on the LED after a while.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 18 replies
  • Answers 8 answers
  • Subscribers 417 subscribers
  • Views 5706 views
  • Users 0 members are here
  • led;
  • time
Related

Turning on the LED after a while.

sonys
sonys over 6 years ago

Hello everyone.

 

The task:

Use the button to turn on and off the LED after a while.

 

For example, we pressed a button - the LED turned on and went out after 10 seconds. And so it should turn itself on every 5 minutes for 10 seconds. Then, press the button and the LED stops working and until the next button press, it does not work.

 

What features are better to use? Or who has a similar example?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +4 suggested
    Hi Sofiia, If you do not need to use an arduino I believe a dedicated circuit using two 555 timers and a flip flop will be able to produce this effect. John
  • shabaz
    shabaz over 6 years ago +3 suggested
    Hi Sofiia, To do this properly is quite an advanced thing. There's a capability inside the Arduino (it is slightly different depending on which Arduino you are using, but at a high level, the concept is…
  • ankur608
    ankur608 over 6 years ago +2 suggested
    For simplicity, you can replace your button with 'push on-off' or add an another 'tact switch' for the same. This will make your code routine much easier. Remember things that can't be reached with just…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Sofiia,

     

    To do this properly is quite an advanced thing. There's a capability inside the Arduino (it is slightly different depending on which Arduino you are using, but at a high level, the concept is the same) called a timer. The timer can be programmed to generate something called an 'interrupt' which calls a special function (called an interrupt service routine) regularly, for example every second.

    Then, you can use a global variable to count these 1-second ticks. Another global variable can be used to store state information related to (say) button press.

    Button-presses need debouncing, that is another topic too,

    To make a long story short, these two topics will require a lot of reading.

    Some resources are here:

    Timers and interrupts: https://learn.adafruit.com/multi-tasking-the-arduino-part-2/timers

    Button debounce: https://blog.adafruit.com/2009/10/20/example-code-for-multi-button-checker-with-debouncing/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sonys
    0 sonys over 6 years ago in reply to shabaz

    I made sketches, look, please. I need to add time, but I'm already confused with the millis () function. Correct, if there's a mistake.

     

    class PauseFlasher
    {
      const unsigned long maxValue = 4294967295UL; // maximum counter value
    
      int ledPin; 
      long OnTime; 
      long OffTime; 
      long PeriodFlashing; 
      long PeriodPause; 
    
      int ledState; 
      int ledFlashing; 
      int keyState, oldKeyState; 
      unsigned long previousMillis;
      unsigned long previousFlashingMillis; 
      unsigned long previousKeyMillis;
    
      public:
      PauseFlasher(int pin, long on, long off, long flashing, long pause)
      {
       ledPin = pin;
       pinMode(ledPin, OUTPUT);
    
       OnTime = on;
       OffTime = off;
       PeriodFlashing = flashing;
       PeriodPause = pause;
    
       ledState = HIGH;
       ledFlashing = HIGH;
       keyState = LOW;
       oldKeyState = HIGH;
       previousMillis = 0; 
       previousFlashingMillis = 0; 
       previousKeyMillis = 0;
      }
    
      void Update()
      {
        unsigned long currentMillis = millis(); 
        unsigned long temp_time=0, temp_time1=0;
    
        if (currentMillis >= previousFlashingMillis) temp_time1 = currentMillis - previousFlashingMillis;
        else temp_time1 = maxValue - previousFlashingMillis + currentMillis;
    
        if ((ledFlashing==HIGH) && (temp_time1 >= PeriodFlashing))
        {
          ledFlashing = LOW; 
          previousFlashingMillis = currentMillis; 
          digitalWrite(ledPin, ledFlashing); 
          keyState = LOW;
          oldKeyState= HIGH;
        }
        if ((ledFlashing==LOW) && (temp_time1 >= PeriodPause))
        {
          ledFlashing = HIGH; 
          previousFlashingMillis = currentMillis ; 
          digitalWrite(ledPin, ledFlashing); 
          keyState = LOW;
          oldKeyState= HIGH;
        }
    
        if(ledFlashing==HIGH)
        {
          if (currentMillis >= previousMillis) temp_time = currentMillis - previousMillis;
          else temp_time = maxValue  - previousMillis + currentMillis;
          
          if((ledState == HIGH) && (temp_time >= OnTime))
          {
            ledState = LOW; // выключаем
            previousMillis = currentMillis; 
            digitalWrite(ledPin, ledState); 
          }
          else if ((ledState == LOW) && (temp_time >= OffTime))
          {
            ledState = HIGH; // включаем
            previousMillis = currentMillis ; 
            digitalWrite(ledPin, ledState); 
          }
        }
        if(ledFlashing==LOW)
        {
          if (digitalRead(2)==HIGH)
          {
            if(millis()-previousKeyMillis>100)
            {
              previousKeyMillis = millis();
              if(keyState==oldKeyState)
              {
                if(keyState==LOW) keyState=HIGH;
                else if(keyState==HIGH) keyState=LOW;
                digitalWrite(ledPin, keyState);
              }  
            }
          }
          else oldKeyState=keyState;
        }
      }
    };
    
    PauseFlasher led1(13, 100, 200, 5000, 15000);
    
    void setup(){}
    
    void loop()
    {
      led1.Update();
    }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to sonys

    Hi Sofiia,

     

    The code is hard to follow, possibly line 54 might need changing from "if" to "else if" but I'm only guessing, I could only partially understand the code.

    You can use Serial.println to print out debug to try to get an idea where the code executes, and the values of variables to debug this, so that you can be sure that the values in the variables are what you expect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sonys
    0 sonys over 6 years ago in reply to shabaz

    Thanks. It remains to understand where to write what numbers (which I need), otherwise I’m already confused. Can you help me please?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sonys
    0 sonys over 6 years ago in reply to shabaz

    Thanks. It remains to understand where to write what numbers (which I need), otherwise I’m already confused. Can you help me please?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 6 years ago in reply to sonys

    There's no guideline on where to write the values, it just needs to be done wherever you suspect (after running the code and seeing the result for example) there could be an error, or wherever you want to be sure the value is changing as expected.

    You can comment them out afterwards if you don't need them after debugging.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer