Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum arduino single signal digital
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 415 subscribers
  • Views 1579 views
  • Users 0 members are here
Related

arduino single signal digital

balexfox
balexfox over 5 years ago

I ask for help I'm not good at Arduino
I need to send a single signal to the outputs only without delay. oscillogram attached time. signal for a certain time high then low then high again. thanks for the help. second signal high then low to the end. thank you

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 5 years ago +1 verified
    Can this help? #define SIGNAL1_PIN 5 #define SIGNAL2_PIN 8 #define SIGNAL1_PULSE_LENGTH_MS 2000 #define SIGNAL2_START_DELAY_MS 500 void setup() { pinMode(SIGNAL1_PIN, OUTPUT); pinMode(SIGNAL2_PIN, OUTPUT…
  • balexfox
    balexfox over 5 years ago in reply to javagoza +1 suggested
    delay is not suitable because it slows down the code and I have a lot of it. Here's an example I don't know how to fix it. unsigned long currentMillis = millis(); unsigned long currentMillis2 = millis…
  • balexfox
    balexfox over 5 years ago in reply to javagoza +1
    thank you very much
Parents
  • javagoza
    0 javagoza over 5 years ago

    Can this help?

     

    #define SIGNAL1_PIN  5
    #define SIGNAL2_PIN  8
    #define SIGNAL1_PULSE_LENGTH_MS 2000
    #define SIGNAL2_START_DELAY_MS 500 
    
    void setup() {
    pinMode(SIGNAL1_PIN, OUTPUT);
    pinMode(SIGNAL2_PIN, OUTPUT);
    digitalWrite(SIGNAL1_PIN, HIGH);
    digitalWrite(SIGNAL2_PIN, HIGH);
    }
    
    void pulseS1LowS2() {
    digitalWrite(SIGNAL1_PIN, LOW);
    delay(SIGNAL2_START_DELAY_MS);
    digitalWrite(SIGNAL2_PIN, LOW);
    delay(SIGNAL1_PULSE_LENGTH_MS - SIGNAL2_START_DELAY_MS);
    digitalWrite(SIGNAL1_PIN, HIGH);
    }
    
    void loop() {
      // call pulseS1LowS2() when needed
    }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balexfox
    0 balexfox over 5 years ago in reply to javagoza

    ok i will try

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balexfox
    0 balexfox over 5 years ago in reply to javagoza

    ok i will try