Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum gear step ratio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 415 subscribers
  • Views 1586 views
  • Users 0 members are here
Related

gear step ratio

balexfox
balexfox over 5 years ago

Hello everyone
help to understand the code
need to increase
pulse_buffer in 1.2
but the code only allows integer 1 2 and so on.
tried changing the pulse_buffer datatype to round off STEPS_PR_ENCODER_PULSE

but it only works equally well with the whole. can still some parameter increase to then divide?

or how it make by another way because its impossible set impulse 1.2

 

#define ENCODER_PULSE_PIN 2
#define ENCODER_DIR_PIN   3
#define DRIVER_STEP_PIN   4
#define DRIVER_DIR_PIN    7
#define DRIVER_EN_PIN     8

#define STEPS_PR_ENCODER_PULSE  1
#define DRIVER_PULSE_PERIOD_US  1

enum Driver_pulse_state_enum {PULSE_IDLE, PULSE_HIGH, PULSE_LOW};  



uint8_t dir = LOW;  
uint16_t pulse_buffer = 0;  
unsigned long time_now = 0;  
uint16_t driver_pulse_hold_time_us = DRIVER_PULSE_PERIOD_US/2;  
uint8_t driver_pulse_state = PULSE_IDLE;  





void setup() {  

  pinMode(ENCODER_PULSE_PIN, INPUT);  
  pinMode(ENCODER_DIR_PIN, INPUT);  
  pinMode(DRIVER_STEP_PIN, OUTPUT);  
  pinMode(DRIVER_DIR_PIN, OUTPUT);  
  pinMode(DRIVER_EN_PIN, OUTPUT);  

  attachInterrupt(digitalPinToInterrupt(ENCODER_PULSE_PIN), encoderISR, RISING);  

  digitalWrite(DRIVER_EN_PIN, HIGH);  





void loop() {  


if((pulse_buffer) && (driver_pulse_state == PULSE_IDLE)){  
    driver_pulse_state = PULSE_HIGH;  
    digitalWrite(DRIVER_DIR_PIN, digitalRead(ENCODER_DIR_PIN));  
    digitalWrite(DRIVER_STEP_PIN, HIGH);  
    time_now = micros();  
  }  

if((micros() - time_now > driver_pulse_hold_time_us) && (driver_pulse_state == PULSE_LOW)){  
    driver_pulse_state = PULSE_HIGH;  
    digitalWrite(DRIVER_STEP_PIN, HIGH);  
    time_now = micros();  
  }  

if((micros() - time_now > driver_pulse_hold_time_us) && (driver_pulse_state == PULSE_HIGH)){  
    digitalWrite(DRIVER_STEP_PIN, LOW);  
    time_now = micros();  

    pulse_buffer -= 1;  
if(pulse_buffer < 0){  
      pulse_buffer = 0;  
    }  

if(pulse_buffer){  
      driver_pulse_state = PULSE_LOW;  
    }  
else{  
      driver_pulse_state = PULSE_IDLE;  
    }  
  }  



}  

void encoderISR(){  
  pulse_buffer += STEPS_PR_ENCODER_PULSE;  
} 

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +3 suggested
    Do you want to use floating point? You have not provided a lot of information on what you are trying to do and floating point seems unusual with an encoder but here are some thoughts: pulse_buffer is in…
  • balexfox
    balexfox over 5 years ago in reply to fmilburn +1
    all control by Accelstepper i get a done code and i dont now why it is not working correctly
  • fmilburn
    fmilburn over 5 years ago in reply to balexfox +1 suggested
    I don’t see AccelStepper in the sketch above so it is not possible to help with that. The problem could be wiring, a problem in the code that isn’t listed above, damaged parts, or any number of other things…
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    Do you want to use floating point?   You have not provided a lot of information on what you are trying to do and floating point seems unusual with an encoder but here are some thoughts:

    • pulse_buffer is in an ISR, it should be declared volatile
    • pulse_buffer is unint16_t so it will be treated as an integer unless it is declared float
    • possibly a cast could be used but it isn’t clear what the objective is
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balexfox
    0 balexfox over 5 years ago in reply to fmilburn

    all control by Accelstepper

    i get a done code

    and i dont now why it is not working correctly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balexfox
    0 balexfox over 5 years ago in reply to fmilburn

    all control by Accelstepper

    i get a done code

    and i dont now why it is not working correctly

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fmilburn
    0 fmilburn over 5 years ago in reply to balexfox

    I don’t see AccelStepper in the sketch above so it is not possible to help with that.  The problem could be wiring, a problem in the code that isn’t listed above, damaged parts, or any number of other things. Much more information would be needed.  First though, rule out everything you can and narrow down the issue.  If it is software then get the Arduino library example working and determine what change makes it break.  Same way with hardware, get the individual pieces working and determine one at a time what addition or piece makes it break.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer