Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Which is the Low cost High Sample rate ADC?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 415 subscribers
  • Views 3764 views
  • Users 0 members are here
  • i2c
  • esp
  • esp-8266
  • esp-32
  • adc
  • arduino-pico
Related

Which is the Low cost High Sample rate ADC?

ajsparks
ajsparks over 5 years ago

I want to sample signals ranging from 0 - 1 MHz. Can you suggest a low-cost ADC with a sample rate > 2 MSPS, having I2C connectivity so that I can get data to Arduino or ESP.

 

Waiting for your suggestions

Thank you in advance. image

  • Sign in to reply
  • Cancel
  • ajcc
    0 ajcc over 5 years ago

    The fastest I²C speed is 5 Mbit/s, even with SPI that only goes up to ~10-20 Mbps or so(?), so you're going to have a really hard time sampling at 2 MSPS.

    But if you just want an "Arduino" that can sample 1 MHz signals, then I'd like to suggest getting a STM32 NUCLEO-F303RESTM32 NUCLEO-F303RE instead. This board has a STM32F303RE µC (microcontroller [unit] or MCU) on it, with really fast 12-bit ADCs inside that can sample at up to 5 MSPS. This µC is part of the STM32 F3 family of mixed-signal µCs and there are other Nucleo boards featuring them (there's a large variety of Nucleo boards and STM32 µCs so be careful to select the right one).

     

    Edit: I noticed the Nucleo I linked first was out of stock, so an alternative could be the STM32 NUCLEO-F334R8STM32 NUCLEO-F334R8 with its STM32F334R8T6STM32F334R8T6 µC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer