Arduino
  • Products
  • More
Arduino
Arduino Forum remote controlled car problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 799 views
  • Users 0 members are here
  • coding
  • maker
  • pins
  • connect
  • help
  • control
  • b
  • separate
  • pot
  • servo
  • code
  • not
  • electrical
  • motor
  • arduino
  • analog
  • remote
  • j
Related

remote controlled car problem

dirtdiver
dirtdiver over 15 years ago

Hello everyone, here is the problem :

I'm making a remote control truck with the Arduino but the analog pins are just not enough.I have 2 analog pins left and I have to control 4 servos with potentiometers.

 

Now, my idea is to use the 1st pin for a pot that is separatet into 4 sections.Each section will connect the pot from the 2nd analog pin to servos 1-4.

I dont know if that is possible so please tell me if I can do that and how to do it.

Also if you can think of something else that solves my problem, feel free to share it!

Thanks for the help!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +1 verified
    i did a similar build for a tech fair wat scale are you aiming for do you want full motor control or just partial
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to dirtdiver +1
    In your "if" condition, do you mean to check the analogRead value of potpin1, instead of just the value of potpin1 (which is always set to 1), like so: if (analogRead(potpin1) > 500){
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    i did a similar build for a tech fair wat scale are you aiming for do you want full motor control or just partial

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 15 years ago in reply to e14 Contributor

    Well here's what I've wrote so far, you will get the idea of what Im tring to do.The code is not working and I dont really know why

     

    Servo myservo;  // create servo object to control a servo
    Servo myservo1;

    int potpin1 = 0;  // analog pin used to connect the potentiometer
    int potpin = 1;
    int val;    // variable to read the value from the analog pin

    void setup()
    {
      myservo.attach(9);  // attaches the servo on pin 9 to the servo object
    myservo1.attach(10);
    }

    void loop()
    {
      if (potpin1 > 500){
       val = analogRead(potpin);            // reads the value of the potentiometer (value between 0 and 1023)
      val = map(val, 0, 1023, 0, 179);     // scale it to use it with the servo (value between 0 and 180)
      myservo.write(val);                  // sets the servo position according to the scaled value
      delay(15);
      } else  {
      val = analogRead(potpin);            // reads the value of the potentiometer (value between 0 and 1023)
      val = map(val, 0, 1023, 0, 179);     // scale it to use it with the servo (value between 0 and 180)
      myservo1.write(val);                  // sets the servo position according to the scaled value
      delay(15);
      }
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to dirtdiver

    In your "if" condition, do you mean to check the analogRead value of potpin1, instead of just the value of potpin1 (which is always set to 1), like so:

     

    if (analogRead(potpin1) > 500){

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to dirtdiver

    In your "if" condition, do you mean to check the analogRead value of potpin1, instead of just the value of potpin1 (which is always set to 1), like so:

     

    if (analogRead(potpin1) > 500){

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dirtdiver
    0 dirtdiver over 15 years ago in reply to e14 Contributor

    Thanks man, it worked when i changed it!