Arduino
  • Products
  • More
Arduino
Arduino Forum any one help me
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 418 subscribers
  • Views 1164 views
  • Users 0 members are here
Related

any one help me

e14 Contributor
e14 Contributor over 14 years ago

i bought UltraSonic Distance Sensor ( Serial Ascii O/p) from rhydolabz.

i connect this sensor to arduino uno board but this sensor didn't give the correct distance

i want arduino program for this sensor.

 

i use this program

 

/* Ping))) Sensor
 
   This sketch reads a PING))) ultrasonic rangefinder and returns the
   distance to the closest object in range. To do this, it sends a pulse
   to the sensor to initiate a reading, then listens for a pulse
   to return.  The length of the returning pulse is proportional to
   the distance of the object from the sensor.
    
   The circuit:
    * +V connection of the PING))) attached to +5V
    * GND connection of the PING))) attached to ground
    * SIG connection of the PING))) attached to digital pin 7

 

   http://www.arduino.cc/en/Tutorial/Ping
  
   created 3 Nov 2008
   by David A. Mellis
   modified 30 Jun 2009
   by Tom Igoe

   This example code is in the public domain.

 

*/

 

// this constant won't change.  It's the pin number
// of the sensor's output:
const int pingPin = 7;

 

void setup() {
  // initialize serial communication:
  Serial.begin(9600);
}

 

void loop()
{
  // establish variables for duration of the ping,
  // and the distance result in inches and centimeters:
  long duration, inches, cm;

 

  // The PING))) is triggered by a HIGH pulse of 2 or more microseconds.
  // Give a short LOW pulse beforehand to ensure a clean HIGH pulse:
  pinMode(pingPin, OUTPUT);
  digitalWrite(pingPin, LOW);
  delayMicroseconds(2);
  digitalWrite(pingPin, HIGH);
  delayMicroseconds(5);
  digitalWrite(pingPin, LOW);

 

  // The same pin is used to read the signal from the PING))): a HIGH
  // pulse whose duration is the time (in microseconds) from the sending
  // of the ping to the reception of its echo off of an object.
  pinMode(pingPin, INPUT);
  duration = pulseIn(pingPin, HIGH);

 

  // convert the time into a distance
  inches = microsecondsToInches(duration);
  cm = microsecondsToCentimeters(duration);
 
  Serial.print(inches);
  Serial.print("in, ");
  Serial.print(cm);
  Serial.print("cm");
  Serial.println();
 
  delay(100);
}

 

long microsecondsToInches(long microseconds)
{
  // According to Parallax's datasheet for the PING))), there are
  // 73.746 microseconds per inch (i.e. sound travels at 1130 feet per
  // second).  This gives the distance travelled by the ping, outbound
  // and return, so we divide by 2 to get the distance of the obstacle.
  // See: http://www.parallax.com/dl/docs/prod/acc/28015-PING-v1.3.pdf
  return microseconds / 74 / 2;
}

 

long microsecondsToCentimeters(long microseconds)
{
  // The speed of sound is 340 m/s or 29 microseconds per centimeter.
  // The ping travels out and back, so to find the distance of the
  // object we take half of the distance travelled.
  return microseconds / 29 / 2;
}

but this program for decimal o/p

but my sensor ASCII output

how can i get decimal value(correct distance)

  • Sign in to reply
  • Cancel
Parents
  • chgus
    0 chgus over 14 years ago

    I had a quick look at the documetation for the sensor You have used. It more or less does it all for You.

    The code You have supplied calculates timing for a much simpler sensor.

     

    You should use Serial or SoftwareSerial to catch the numbers Your sensor are sending, byte by byte.

    SoftwareSerial works up to 9600 baud - the same speed your sensor sends data.

     

    Try something like this to see the output from Your sensor relayed:

    (since I have no sensor hardware available, I was not able to test it live.)

     

    // Echo sonic sensor output to console output

    #include <SoftwareSerial.h>
    #define sonicPin 7
    #define notused_tx 8
    SoftwareSerial sonic = SoftwareSerial(sonicPin,notused_tx);
    void setup() {
      // initialize serial communication:
      Serial.begin(9600);
      // initialize serial comm from sensor:
      pinMode(sonicPin,INPUT);
      // sensor send chars at 9600 baud
      sonic.begin(9600);
    }
    void loop()
    {
      char buffer[20];
      int i=0;
      char c='.';
      // read and buffer sensor output
      while((c=sonic.read()) != 0xd){
        buffer[i++]=c;
      }
      buffer[i]=0;
      Serial.println(buffer);
    }

    #include <SoftwareSerial.h>

    #define sonicPin 7

    #define notused_tx 8

    SoftwareSerial sonic = SoftwareSerial(sonicPin,notused_tx);

     

    void setup() {

      // initialize serial communication:

      Serial.begin(9600);

      // initialize serial comm from sensor:

      pinMode(sonicPin,INPUT);

      // sensor send chars at 9600 baud

      sonic.begin(9600);

    }

     

    void loop()

    {

      char buffer[20];

      int i=0;

      char c;

      // read and buffer sensor output

      while((c=sonic.read()) != 0xd){

        buffer[i++]=c;

      }

      buffer[i]=0;

      Serial.println(buffer);

    }

     

    Hope this helps image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • chgus
    0 chgus over 14 years ago

    I had a quick look at the documetation for the sensor You have used. It more or less does it all for You.

    The code You have supplied calculates timing for a much simpler sensor.

     

    You should use Serial or SoftwareSerial to catch the numbers Your sensor are sending, byte by byte.

    SoftwareSerial works up to 9600 baud - the same speed your sensor sends data.

     

    Try something like this to see the output from Your sensor relayed:

    (since I have no sensor hardware available, I was not able to test it live.)

     

    // Echo sonic sensor output to console output

    #include <SoftwareSerial.h>
    #define sonicPin 7
    #define notused_tx 8
    SoftwareSerial sonic = SoftwareSerial(sonicPin,notused_tx);
    void setup() {
      // initialize serial communication:
      Serial.begin(9600);
      // initialize serial comm from sensor:
      pinMode(sonicPin,INPUT);
      // sensor send chars at 9600 baud
      sonic.begin(9600);
    }
    void loop()
    {
      char buffer[20];
      int i=0;
      char c='.';
      // read and buffer sensor output
      while((c=sonic.read()) != 0xd){
        buffer[i++]=c;
      }
      buffer[i]=0;
      Serial.println(buffer);
    }

    #include <SoftwareSerial.h>

    #define sonicPin 7

    #define notused_tx 8

    SoftwareSerial sonic = SoftwareSerial(sonicPin,notused_tx);

     

    void setup() {

      // initialize serial communication:

      Serial.begin(9600);

      // initialize serial comm from sensor:

      pinMode(sonicPin,INPUT);

      // sensor send chars at 9600 baud

      sonic.begin(9600);

    }

     

    void loop()

    {

      char buffer[20];

      int i=0;

      char c;

      // read and buffer sensor output

      while((c=sonic.read()) != 0xd){

        buffer[i++]=c;

      }

      buffer[i]=0;

      Serial.println(buffer);

    }

     

    Hope this helps image