Arduino
  • Products
  • More
Arduino
Arduino Forum SD Card interface board made by LC Studio/lcsoft.net
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 43 replies
  • Answers 2 answers
  • Subscribers 422 subscribers
  • Views 7722 views
  • Users 0 members are here
  • aduino
  • sd_card
  • uno
Related

SD Card interface board made by LC Studio/lcsoft.net

neilk
neilk over 14 years ago

I am trying to get the above SD Card interface board working with my Arduino UNO. The interface board includes a 5v to 3.3v regulator and appears to have appropriate resistors to cope with 5v signals from the UNO.


The pinout on the board is not directly compatible with the header on the UNO, so I have made up some connectors and I am fairly sure I have made the connections to the SPI correctly:

 

I/F Board     Arduino Pin

CS               10

MOSI           11

SCK            13

MISO           12

 

I have tried supplying +5v, to derive 3.3v via the I/F card regulator and also supplied +3.3v directly.

 

My test program fails to find the card and returns "Card Failure", irrespective of whether there is a card present or not.

The card I am using is 2GB, formatted as FAT16 and contains a single file - "test.txt", the contents of which are simply:

test1,test2

I keep checking the card in a reader on my PC and, so far, I don't seem to have damaged it.

 

I would be grateful for any advice, please.

 

A fragment of the program is shown below:

 

//Program by Jeremy Blum

//www.jeremyblum.com

//SD Card Demonstration

//Based on Example by Tom Igoe

//Further adapted simplified by NGK to try and prove my SD Card interface board actually works!!!

 

#include <SD.h> // This is the standard SD library in version 0023

 

//These values are used by default in the standard SD Card Library

//MOSI = 11

//MISO = 12

//SCLK = 13

 

//We need to set the CS Pin - it's 10 for the UNO

int CS_pin = 10;

 

void setup()

{

  Serial.begin(9600);

  Serial.println("Initializing Card");

  //CS Pin is an output

  pinMode(CS_pin, OUTPUT);

 

  if (!SD.begin(CS_pin))

  {  

   Serial.println("Card Failure");

   return;

   }

 

  Serial.println("Card Ready");

 

  //Now read the File test.txt)

  File commandFile = SD.open("test.txt");

  if (commandFile)

  {

    Serial.println("Reading Command File");

    while(commandFile.available())

    {

      char temp = (commandFile.read());

      Serial.println(temp);

     }

  }

  else

  {

    Serial.println("Could not open command file.");

    return;

  }

}

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 14 years ago +1 suggested
    Hi - I tried looking up the module put couldn't find much detail on the board (that translated to English with Google at least). One idea I had from working with other 3.3V modules is that logic level…
  • fustini
    fustini over 14 years ago in reply to neilk +1 suggested
    Yeah, I think the issue is 3.3V & 5V interfacing. I'm not sure if the resistor method is very good per this advice from Adafruit: http://www.ladyada.net/products/microsd/ One is that they are strictly…
  • nermash
    nermash over 14 years ago in reply to neilk +1
    According to specs at http://www.arduino.cc/en/Main/arduinoBoardUno digital IOs operate at 5 volts, so you need apropriate level shifter/buffer for SI line on the uno board. I had a simillar problem interfacing…
Parents
  • fustini
    0 fustini over 14 years ago

    Hi -

     

    I tried looking up the module put couldn't find much detail on the board (that translated to English with Google at least).  One idea I had from working with other 3.3V modules is that logic level shifting (e.g. converter) might be necessary.  I believe the Arduino UNO runs at 5V so this could be an issue.

     

    I ran into this when working with interfacing an Arduino with a 3.3V Microchip SRAM chip.  SparkFun has a nice tutorial called "Sensor Interfacing" that describes different solutions to this issue:

     

    http://www.sparkfun.com/tutorials/65

     

    I ended up ordering SparkFun's little converter boards which worked very well:

     

    http://www.sparkfun.com/products/8745

     

     

    Cheers,

    Drew

    http://twitter.com/pdp7

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • harbo
    0 harbo over 14 years ago in reply to fustini

    Drew, how did you make the connection from the Arduino [SCK-MISO-MOSI-CS] to the 8745{RX, TX]  ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to harbo

    Hi Harrie,

     

    I think I've since disconnected it but I'll have a look tonight.  I remember there was a bit of trial and error - wish I would have documented it better (last worked on it in February).

     

    Cheers,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • harbo
    0 harbo over 14 years ago in reply to fustini

    and Drew, did you find the something?

     

    Cheers

     

    Harrie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to harbo

    Hi Harrie,

     

    Sorry this slipped by my mind before I left for a wedding in Canada.  I'll check tonight.

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to fustini

    Hi Harrie -

     

    Sadly, my project has been dismantled so I can't recollect.  But I hooked it up based on advice I read on arduino.cc forum.  Were you able to get it working?

     

    Thanks,

    Drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • harbo
    0 harbo over 14 years ago in reply to fustini

    Drew,

     

    Finale I got it working, attached the scheme I used. But.....The SD, apart,

    is working, and the Max31855 Temperature read-out also apart working. But

    together .....Noy yet.

    I'm not real a C-specialist, so I'm struggling with SPI now.

     

     

    2011/12/12 Drew Fustini <messages@element14.com>

     

    **

        image: element14<http://www.element-14.com?CMP=e14notificationemail_header> Re: SD Card interface board made by LC Studio/

    lcsoft.net  created by Drew Fustini<http://www.element14.com/community/people/fustini>in

    Arduino Projects | Arduino Programming - View the full discussion<http://www.element14.com/community/message/41273#41273/l/re-sd-card-interface-board-made-by-lc-studiolcsoftnet

     

    Attachments:
    imageBOB8745_MAX31855.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • r3cgm
    0 r3cgm over 14 years ago in reply to harbo

    I'm in the same boat as Neil.  Same pin connections (tried CS on both pin 10 and pin 4), and the CardInfo diagnostic program still returns:

     

    Initializing SD card...initialization failed. Things to check:
    * is a card is inserted?
    * Is your wiring correct?
    * did you change the chipSelect pin to match your shield or module?

    Initializing SD card...initialization failed. Things to check:

    * is a card is inserted?

    * Is your wiring correct?

    * did you change the chipSelect pin to match your shield or module?

    Anyone else have success with this component from LC Studio?  Is the 3.3V conversion with a 74HC4050 really needed?  Any tips appreciated.
    Christopher

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neilk
    0 neilk over 14 years ago in reply to r3cgm

    Hi Christopher - I have spent hours trying to get this to work, including building a 5v to 3.3v logic conversion with a 74HC4050 (sourcing that at a sensible price is another story!)

    Out of sheer frustration, I took a meter to the LC Studio board (unplugged from my arduino stuff). What I appeared to find confused me - MISO and MOSI were both shorted to ground ??

    I suspected the soldering around the card socket & so went over with very carefully and eventually unsoldered it, damaging it in the process. I then scraped off the protective layers from areas of the PCB and tried to follow the copper - I found what appeared to be shorts in the copper and so tried to scrape them away.

     

    In short, I virtually destroyed the board, but more or less convinced myself that it was originally faulty. Christmas and New Year have intervened and I am only just picking up the Arduino project again. I haven't yet communicated with the (eBay) seller, but am wondering what can be done........It would cost me more to return the board (to the far east) than I paid for it.

     

    Just to buy an SD Card connector (I mean 1, not 100 or 10,000) is ridiculously expensive, so I am now contemplating cannibalising a USB/SD Card reader.

     

    I would be fascinated to know if your LC Studio board shows the same symptoms as mine??

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terryking
    0 terryking over 14 years ago in reply to neilk

    Hi, I had similar problems with a different SD Card module. I found these that use FETs for level translation and include a 3.3V regulator set up to run on both 5V Arduinos etc. and 3.3V controllers:

     

    http://arduino-direct.com/sunshop/index.php?l=product_detail&p=246

     

    I now stock these for $9.50   DISCLAIMER: Mentioned stuff from my own shop...!! Which is what I know most about :-)

     

    Regards, Terry King  ...On the Mediterranean in Italy  terry@yourduino.com

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • terryking
    0 terryking over 14 years ago in reply to neilk

    Hi, I had similar problems with a different SD Card module. I found these that use FETs for level translation and include a 3.3V regulator set up to run on both 5V Arduinos etc. and 3.3V controllers:

     

    http://arduino-direct.com/sunshop/index.php?l=product_detail&p=246

     

    I now stock these for $9.50   DISCLAIMER: Mentioned stuff from my own shop...!! Which is what I know most about :-)

     

    Regards, Terry King  ...On the Mediterranean in Italy  terry@yourduino.com