Arduino
  • Products
  • More
Arduino
Arduino Forum transistor used as a button
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 2430 views
  • Users 0 members are here
  • keyboard
  • help
  • arduino
Related

transistor used as a button

dirtdiver
dirtdiver over 14 years ago

Hi,

Im using a transistor as a button that is pressing a button on  a  hacked keyboard.

Heres how the hacked  keyboard works (that is the small PCB iside the keyboard)-

image

Now what I want to do is use a transistor to connect the pins and get a letter.Heres how i did it .My questios is it correct couse im having some issues

with it like getting random letters or not getting any at all.

image

  • Sign in to reply
  • Cancel
Parents
  • YT2095
    0 YT2095 over 14 years ago

    it`s not a Bad idea, but the use of a 4016 or 4069 would have probably been better and more like an actual switch.

    you`ll have to get the timing right too (within reason) else you could either Miss the scan or hit it twice for instance.

    it May be an idea to also bias the transistors base down to deck to preclude any spurious triggerings/noise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    The 4016 is a great idea- exactly the thing I was looking for.I will see if I can find one..or two couse i need like 7 of these.

    So this works like a switch - two pins for  pin4 and pin5 and a 3rd pin going into a digital pin, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    The 4016 is a great idea- exactly the thing I was looking for.I will see if I can find one..or two couse i need like 7 of these.

    So this works like a switch - two pins for  pin4 and pin5 and a 3rd pin going into a digital pin, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • YT2095
    0 YT2095 over 14 years ago in reply to dirtdiver

    yes, it`s just like your transistor idea in principal, but will be seen more like a propper key press, and of course it`s bi-directional, so it doesn`t matter what side goes to where (unlike a transistor).

    the 74125 will do the same and there is 6 of them on a chip, but these Are directional, so you`ll need to know the Scan lines from the inputs, and of course these are 5v only devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer