Arduino
  • Products
  • More
Arduino
Arduino Forum Xbee configuration
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 3 answers
  • Subscribers 418 subscribers
  • Views 1525 views
  • Users 0 members are here
Related

Xbee configuration

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

I'm new to Arduino World. My project is using an Arduino as datalogger for gaz, water and electricity consumption.

In most cases the different counters are not located in the same room. So I have to transmit data from several Arduino's to a an Arduino Master which transmits data over internet.

 

I try to configure the 2 Xbees S2 like explained in the Jeremy’s tutorial : http://www.jeremyblum.com/2011/02/27/arduino-tutorial-9-wireless-communication/

I follow exactly the procedure : 2 jumpers placed correctly, Atmega chip removed. The arduino board is well recognized on COM6 – I use Putty.

 

I enter +++ to communicate with Xbee. I receive OK. Up to there non problem.

AT OK

ATMY : receive FFFE

ATMY1000 : receive ERROR

ATDL1001 : OK

ATID1111, : OK

 

I have understood that the procedure could be different on XBEE S2 models. But I do not understand what parameters I must enter on each device. Xbee 1 must send data to Xbee 2

 

With Xbee 1 :

ATSH returns 13A200

ATSL returns 40612FEC

 

With Xbee 2 :

ATSH returns 13A200

ATSL returns 4061318A

 

Do you have a suggestion ?

Thanks for your help

  • Sign in to reply
  • Cancel
Parents
  • dirtdiver
    0 dirtdiver over 14 years ago

    Are you using the usb explorer. Im going to buy xbees but i dont know if i have to get that explorer too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dirtdiver
    0 dirtdiver over 14 years ago

    Are you using the usb explorer. Im going to buy xbees but i dont know if i have to get that explorer too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to dirtdiver

    Hello Dirtdiver,

     

    I have only 2 Arduino Uno and 2 Xbee Shields.

    I would like to buy an Xbee Explorer but I can not find it in stock.

     

    But it seems that it is possible to program Xbee without Xbee Explorer, following the procedure described in the tutorial :

    http://www.jeremyblum.com/2011/02/27/arduino-tutorial-9-wireless-communication/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I'm having a really hard time establishing any connection. I have an Xbee shield V2.0, and the jumpers are completely different. I don't want to get a separate piece such as the explorer just to get started! Surely there is a way to program an RFbee from the shield?