Arduino Forum Using ATMega32 instead of ATMega328 chip
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 402 subscribers
  • Views 1576 views
  • Users 0 members are here
  • atmega32
  • aurdino
  • arduino_development_environment
  • atmel
Related

Using ATMega32 instead of ATMega328 chip

Former Member
Former Member over 13 years ago

We are doing a project on getting the temperature and humidity details from sensors, displaying it on LCD, and sending it wirelessly using Xbee to another Arduino module to get processed and displayed. For the first part we have written the program in C for the chip ATMega32 not for ATMega328, and simulated in Proteus. Can you tell me whether there is an Arduino kit for this particular IC ATmega32? We have written the code for the second part (Processing and displaying it, may be we will include sending the data using GSM) also in C. For this part we wish to use ATMega328 and Arduino kit. But can we burn this C program into the IC using Aurduino Uno kit? What is the difference between the programming in Arduino kit and C program?

We are beginners and it would be really helpful if you can clear our queries.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    There is a board called Sanguino (www.saguino.cc) which uses the ATMega644p. This chip has 64K flash and IIRC the same pinout as an ATMega32.

    Check out their site, there's a comparison between the Arduino and the Sanguino and also (under 'useit') software and how to install it in the Arduino IDE (boards.txt)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    There is a board called Sanguino (www.saguino.cc) which uses the ATMega644p. This chip has 64K flash and IIRC the same pinout as an ATMega32.

    Check out their site, there's a comparison between the Arduino and the Sanguino and also (under 'useit') software and how to install it in the Arduino IDE (boards.txt)