Arduino
  • Products
  • More
Arduino
Arduino Forum read encoder (motor axis speed)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 2641 views
  • Users 0 members are here
Related

read encoder (motor axis speed)

e14 Contributor
e14 Contributor over 14 years ago

hello,

 

I have an DC motor which is provided with an encoder, this encoder should give a number of pulses per rotation, the encoder provides four pulses per rotation. The maximum motor speed is 1500rpm so this is 25 Hz. The encoder gives 100 pulses a second on this speed.

 

My question is, does anyone have a simple program to read these pulses on the arduino uno? Do I need to read those pulses with a interrupt? How do I do it? I don't have to know the position and the direction of the axis, I only need te speed of it.

 

When I have the speed of the axis in pulses/second I use the speed for a PID regulator on the arduino controller.

 

thx

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 14 years ago +1
    Jeroen, This is easy, start here: http://arduino.cc/playground/Main/RotaryEncoders What is the current draw on the motor? Cabe http://twitter.com/Cabe_e14
Parents
  • DAB
    0 DAB over 14 years ago

    Hi Jeroen,

     

    Most encoders use a byphase Quadrature encoding so you get both position increments and direction of rotation.  You can use a simple circuit to convert it to pulse and direction inputs.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 14 years ago in reply to DAB

    Is the encoder an electrically separate part of the motor assembly?  I assume it requires 4 wires: Vcc, Ground, S1, and S2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 14 years ago in reply to DAB

    Is the encoder an electrically separate part of the motor assembly?  I assume it requires 4 wires: Vcc, Ground, S1, and S2.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to billabott

    thx for the reply!

     

    the encoder is a 4 wire encoder, Vcc, GND, A-,B- chanal.

    I think that this program wil count the pulses every half a second.

     

    const int Encoder_Pin = 2; // output of encoder to interrupt #0, pin 2 of arduino

    int Encoder_Count = 0;

    long Time1 = 0;

    long Time2 = 0;

    long Time3 = 0;

     

    void setup()

    {

     

      Serial.begin(9600);

      attachInterrupt(0, Count_Pulses, FALLING); //attach interrupt to encoder pin

    }

     

    void Count_Pulses()

    {

      //this is the function that runs every time pin 2

      //switches from high to low

      Encoder_Count++;

    }

     

    void loop()

    {

      Time1 = millis();

      Time3 = Time1 -= Time2;

     

      if (Time3 >= 500)

      {

       

       Time2 = millis ();

       int PulsSpeed = Encoder_Count;

       Encoder_Count = 0;

       Serial.println(PulsSpeed);

     

      }

    }