Arduino
  • Products
  • More
Arduino
Arduino Forum read encoder (motor axis speed)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 2645 views
  • Users 0 members are here
Related

read encoder (motor axis speed)

e14 Contributor
e14 Contributor over 14 years ago

hello,

 

I have an DC motor which is provided with an encoder, this encoder should give a number of pulses per rotation, the encoder provides four pulses per rotation. The maximum motor speed is 1500rpm so this is 25 Hz. The encoder gives 100 pulses a second on this speed.

 

My question is, does anyone have a simple program to read these pulses on the arduino uno? Do I need to read those pulses with a interrupt? How do I do it? I don't have to know the position and the direction of the axis, I only need te speed of it.

 

When I have the speed of the axis in pulses/second I use the speed for a PID regulator on the arduino controller.

 

thx

  • Sign in to reply
  • Cancel

Top Replies

  • Catwell
    Catwell over 14 years ago +1
    Jeroen, This is easy, start here: http://arduino.cc/playground/Main/RotaryEncoders What is the current draw on the motor? Cabe http://twitter.com/Cabe_e14
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    HI

    as a fan of the inovative solution the AS5043ASSUAS5043ASSU looks really interesting  for rotary position encoding!!!

     

    The chip data is a http://www.austriamicrosystems.com/Products/Magnetic-Encoders/Rotary-Encoders/AS5043

     

    and three is a realy interesting write up/discussion at http://dangerousprototypes.com/forum/viewtopic.php?f=56&t=3669

     

    Over engineering ? perhaps , cool solution most definitely !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    HI

    as a fan of the inovative solution the AS5043ASSUAS5043ASSU looks really interesting  for rotary position encoding!!!

     

    The chip data is a http://www.austriamicrosystems.com/Products/Magnetic-Encoders/Rotary-Encoders/AS5043

     

    and three is a realy interesting write up/discussion at http://dangerousprototypes.com/forum/viewtopic.php?f=56&t=3669

     

    Over engineering ? perhaps , cool solution most definitely !