Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Midas I2C LCDs
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 8 answers
  • Subscribers 421 subscribers
  • Views 5477 views
  • Users 0 members are here
  • lcd
  • i2c
  • arduino
Related

Midas I2C LCDs

Workshopshed
Workshopshed over 14 years ago

Has anyone tried connecting up one of these I2C LCDs to their Arduino?

 

MIDAS - MCCOG21605B6W-BNMLWIMCCOG21605B6W-BNMLWI - LCD, COG 2X16, NEG STN, W B/L, I2C  - Order Code: 20632092063209

 

 

 

I've got as far as looking at the Wire library http://arduino.cc/it/Reference/Wire and the LCD hardware page http://arduino.cc/playground/Code/LCD  and reading http://www.robot-electronics.co.uk/acatalog/I2C_Tutorial.html

 

I've also watched Jeremy's videos but they are not totally relavent as they are looking at different things

http://www.element14.com/community/videos/3015/l/tutorial-13-for-arduino-liquid-crystal-displays

http://www.element14.com/community/videos/1828/l/Tutorial-07-for-Arduino:-I2C-and-Processing

 

I think I'm happy with the wiring it up, pull up resistors etc. I'm also guessing it will require an external psu to be hooked up.

 

I've not yet ordered the display so it might be straight forward when I get it but just getting as much help as I can before getting going.

  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 14 years ago +3 verified
    I got this working just fine. There were a couple of things I needed to do, firstly, for this particular model, Midas told me the backlight needs to be on for the text to be visible. I also had some fun…
  • Workshopshed
    Workshopshed over 14 years ago in reply to bobcroft +1 suggested
    Bill, I'm only using one display so don't need a multiplexer or switch but it's good to know those exist. Bob, cheers for the link, it's not working just this second but I'll check it out again. It's good…
  • fustini
    fustini over 14 years ago in reply to billabott +1
    Thanks for the link. I'm thinking this would be useful for embedded Linux computers, too, like the Raspberry Pi which have I2C but limited GPIO.
Parents
  • bobcroft
    0 bobcroft over 14 years ago

    Hi Andy, I do not have experience of the particular set up you mention.  However, I have recently added an I2C driven LCD to a project using a 'backpack'.  This works absolutely brilliantly with only two connecctions to the 'duino + power of course, no pull up resistors are used and i used a 20 * 4 LCD.  Backpack comes from www.hobbyelectronics.co.uk and costs £8.00 + £2.00 P+P.  I have no connection to this company and thier service is excellent.

    The backpack PCB comes assembled and with the necessary headers to connect it to a LCD with in line connections.   There is also an Arduino library and example software on the web site.  If you use Arduino 1.0 you will have to change a few bits of code in the library.

     

    I am extremely pleased with this product and it works well leaving my ;duino I/O for other things.

     

    Hope this helps

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • bobcroft
    0 bobcroft over 14 years ago

    Hi Andy, I do not have experience of the particular set up you mention.  However, I have recently added an I2C driven LCD to a project using a 'backpack'.  This works absolutely brilliantly with only two connecctions to the 'duino + power of course, no pull up resistors are used and i used a 20 * 4 LCD.  Backpack comes from www.hobbyelectronics.co.uk and costs £8.00 + £2.00 P+P.  I have no connection to this company and thier service is excellent.

    The backpack PCB comes assembled and with the necessary headers to connect it to a LCD with in line connections.   There is also an Arduino library and example software on the web site.  If you use Arduino 1.0 you will have to change a few bits of code in the library.

     

    I am extremely pleased with this product and it works well leaving my ;duino I/O for other things.

     

    Hope this helps

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Workshopshed
    0 Workshopshed over 14 years ago in reply to bobcroft

    Bill, I'm only using one display so don't need a multiplexer or switch but it's good to know those exist.

     

    Bob, cheers for the link, it's not working just this second but I'll check it out again. It's good to look at the different libraries as they have comments and different techniques for the same areas of control.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer