Arduino
  • Products
  • More
Arduino
Arduino Forum The  L293B  issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 417 subscribers
  • Views 1268 views
  • Users 0 members are here
  • help
  • drive
  • l263b
  • motor
  • arduino
Related

The  L293B  issue

dirtdiver
dirtdiver over 14 years ago

Hi, im trying to use the L29 with only one (PWM) digital pin.

  normaly Pin 2 and Pin 7 go to digital pins on the arduino and they determine the spin direction. image

The code is aways one high and one low -  meaning that pin2 gets 5 volts and pin7 gets 0 volts or vice versa.

Now i dont need to change directions of the rotation, Can i just hook up pin 2 to 5 volts and leave pin 7 free (or should i connect it to ground)

I have tried whats shown in the picture above, but it doesnt work.

Also I am only running one motor, the other side of the chip doent need to be connected to anything right?

Where could be the problem?

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • dirtdiver
    dirtdiver over 14 years ago in reply to dirtdiver +3
    here is the finale version of the project http://www.youtube.com/watch?v=zkptoIx9kSA
Parents
  • dirtdiver
    0 dirtdiver over 14 years ago

    Thanks to billabott , i have completed my project, the working schematic for the L29 is

    image

    I will post a link for you guys to see my project soon!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dirtdiver

    here is the finale version of the project

     

    http://www.youtube.com/watch?v=zkptoIx9kSA

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 14 years ago in reply to dirtdiver

    That is really cool!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 14 years ago in reply to dirtdiver

    That is really cool!!