Arduino
  • Products
  • More
Arduino
Arduino Forum Control Arduino with audio?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 418 subscribers
  • Views 1740 views
  • Users 0 members are here
  • audio
  • arduino
  • iphone
Related

Control Arduino with audio?

JosephFTaylor
JosephFTaylor over 14 years ago

I was wondering if it was possible to connect an audio source to an Arduino with a 3.5mm cable (i.e. iPhone) and play different sounds that the Arduino would recognise to carry out different tasks. I have an Arduino Uno.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • simon.monk
    simon.monk over 14 years ago +1
    Yes, it is. I do just that but for Android rather than iPhone in my book 'Arduino + Android Projects for the Evil Genius'. One-way from the Android tablet to the Arduino in my case, but 2-way is possible…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You could always build a clap circuit with an opamp to take an audio signal and pull one of the arduino pins high. Then based on the number of times the pin is pulled high it can perform different functions…
Parents
  • simon.monk
    0 simon.monk over 14 years ago

    Yes, it is. I do just that but for Android rather than iPhone in my book 'Arduino + Android Projects for the Evil Genius'. One-way from the Android tablet to the Arduino in my case, but 2-way is possible too.

     

    Its the same idea as the old casette tape interfaces that you used to get on home computers. In fact, if you hunt around you can find circuits for a lot of these old computers. I experimented with the circuit from a ZX81, but found it unreliable and ended up making something more complex with an op amp that was a lot more tollerant of the output volume etc.

     

    My publisher wouldn't like it if I gave the schematic, but the Arduino and Android programs are both open source, you can find them on the downloads page here: http://www.duinodroid.com

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • simon.monk
    0 simon.monk over 14 years ago

    Yes, it is. I do just that but for Android rather than iPhone in my book 'Arduino + Android Projects for the Evil Genius'. One-way from the Android tablet to the Arduino in my case, but 2-way is possible too.

     

    Its the same idea as the old casette tape interfaces that you used to get on home computers. In fact, if you hunt around you can find circuits for a lot of these old computers. I experimented with the circuit from a ZX81, but found it unreliable and ended up making something more complex with an op amp that was a lot more tollerant of the output volume etc.

     

    My publisher wouldn't like it if I gave the schematic, but the Arduino and Android programs are both open source, you can find them on the downloads page here: http://www.duinodroid.com