Arduino
  • Products
  • More
Arduino
Arduino Forum Serial Config help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 31 replies
  • Subscribers 420 subscribers
  • Views 4929 views
  • Users 0 members are here
Related

Serial Config help.

YT2095
YT2095 over 14 years ago

I need to configure the Serial on an Arduino to match a very strange Printer, I`m not even sure it`s possible with an Arduino?

it needs to be:

 

1200 Baud

1 Start bit

7 Data bits (LSB first)

1 Parity Bit (Even)

and 2 Stop Bits.

 

Does anyone know how config for this in Arduino, or even if it`s possible?

 

Thanks image

  • Sign in to reply
  • Cancel

Top Replies

  • R_Phoenix
    R_Phoenix over 14 years ago in reply to billabott +1
    SoftwareSerial is no different than useing the built in Serial port. I don't know of anything that even still uses the start bit. As far as I know, the serial port on an Arduino is only 3 wires, RX, TX…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Ah, I see another problem.

     

    Salvador's "how to set the 7 bit" thing only will work on the original hardware serial port .

     

    OP is trying to do serial on pins 2 & 3.

     

    If you can not put the printer on a hardware serial port, you probably have to write your own (software) serial library -- I'm not aware of any of the software serial versions that support 7 bits and even parity.

     

    No worries -- it is not that hard -- 90% of what you need is available open source, only the partity and adding a second stop bit are required to be added; reduce the sent bits from 8 to 7, change time delay to what you need for 1200 bps. You don't even need the receive code. That is harder to do reliably anyway. Sending is easy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 14 years ago in reply to e14 Contributor

    Good catch, so setting UCSR0C only works if using pins 0 and 1? Haven't used those in a while, so correct me if these do not correspond to the original hardware serial port. Nevermind - I've got the Arduino in front of me and just checked it. RX and TX are clearly labeled for pins 0 and 1, respectively. Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • SGarciaV
    0 SGarciaV over 14 years ago in reply to e14 Contributor

    Good catch, so setting UCSR0C only works if using pins 0 and 1? Haven't used those in a while, so correct me if these do not correspond to the original hardware serial port. Nevermind - I've got the Arduino in front of me and just checked it. RX and TX are clearly labeled for pins 0 and 1, respectively. Salvador