Arduino
  • Products
  • More
Arduino
Arduino Forum Beginner Arduino related Questions regarding what hardware to buy..
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 419 subscribers
  • Views 840 views
  • Users 0 members are here
Related

Beginner Arduino related Questions regarding what hardware to buy..

e14 Contributor
e14 Contributor over 14 years ago

Hi everybody,

 

I am a newb to the whole Arduino world and now I want to learn and use. I will start with learning simple stuff but eventually I want to build something as explained later. I have done some soldering before and I am comfortable with it. I am planning to make a project which involves use of GPS sensor, 3 Axis accelerometer, reed switch, couple of IR sensors for distance measurement and a data logger (sd/micro-sd) to record all of the sensors data. The data will be recorded continuously when in operation. It will be portable (i.e. outdoor use and not connected to a computer when using) and will run on batteries.

 

First of all can Arduino do this kind of job? If yes, than can you suggest the types of boards, sensors, shields, otterbox I should buy which can rightnow help me learn building beginner arduino projects and in the end I can also make the abovementioned project. I am aware that some sensors will run on 5V while others on 3.3V which will need shifting so can you also help me choose parts which can do this? I have to (and willing to) buy all the parts together in advance as I will get reimbursed (upto certain amount) from my university. I would love to hear your expert comments as well.

 

Thanks for your help in advance.

  • Sign in to reply
  • Cancel
Parents
  • YT2095
    0 YT2095 over 14 years ago

    another thing worth a mention is that although the DIP version of the 328p sush as that on the Uno will probably have enough pins to all those things you want, if you get a board with the Surface mount version of the 328p you get 2 extra I/O pins on the analog side image

    all boards that I`v seen have a 3.3v supply on them as well, so you should be o.k there as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • YT2095
    0 YT2095 over 14 years ago

    another thing worth a mention is that although the DIP version of the 328p sush as that on the Uno will probably have enough pins to all those things you want, if you get a board with the Surface mount version of the 328p you get 2 extra I/O pins on the analog side image

    all boards that I`v seen have a 3.3v supply on them as well, so you should be o.k there as well.