Arduino
  • Products
  • More
Arduino
Arduino Forum Beginner Arduino related Questions regarding what hardware to buy..
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 419 subscribers
  • Views 838 views
  • Users 0 members are here
Related

Beginner Arduino related Questions regarding what hardware to buy..

e14 Contributor
e14 Contributor over 14 years ago

Hi everybody,

 

I am a newb to the whole Arduino world and now I want to learn and use. I will start with learning simple stuff but eventually I want to build something as explained later. I have done some soldering before and I am comfortable with it. I am planning to make a project which involves use of GPS sensor, 3 Axis accelerometer, reed switch, couple of IR sensors for distance measurement and a data logger (sd/micro-sd) to record all of the sensors data. The data will be recorded continuously when in operation. It will be portable (i.e. outdoor use and not connected to a computer when using) and will run on batteries.

 

First of all can Arduino do this kind of job? If yes, than can you suggest the types of boards, sensors, shields, otterbox I should buy which can rightnow help me learn building beginner arduino projects and in the end I can also make the abovementioned project. I am aware that some sensors will run on 5V while others on 3.3V which will need shifting so can you also help me choose parts which can do this? I have to (and willing to) buy all the parts together in advance as I will get reimbursed (upto certain amount) from my university. I would love to hear your expert comments as well.

 

Thanks for your help in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Thanks guys for your replies and great suggestions.... I will start with the breadboard approach as mentioned by terry king to see if my circuit works as intended before soldering everything. I have decided to buy Uno R3 board but I am not 100% sure if it will accomodate all the i/o s for my project. Can somebody help me with this? Also I need help selecting a data loggers which can easily mount on the Uno. Can I buy a single data logger which can write data from all the sensors in log files simultaneously? Or should I buy different data logger for each sensor? Also can you explain how data loggers work?

     

    I have two IR sensors made by Sharp, one for long range and one for short... GP2Y0A710K0F (LR) and GP2Y0A02YK0F (SR) with analog outputs for both of them.

    I havn't selected a GPS module yet but it will have one digital output.

    3 axis-accelerometer (not selected) will have 3 analog or PWM outputs.

    Reed switch will also have one digital or analog (not sure) output.

    All of the above with the data logger shield/shields.

     

    So do I have enough i/o if I go for Uno R3?

     

    Also I wanted to know little bit about stacking and prototype boards, i.e. How many maximum number of boards I can stack on UNO. Is it advisable to stack them with prototypes or should I solder them? Can you suggest some baords with 3 axis accelerometers and GPS module?

     

    Thanks again for your support and sorry for so many new questions? As I said I am a noob...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    it should relatively easily accomodate all those devices and maybe have a couple spare, assuming of course that your GPS is serial out.

    you have 19 pins, 6 of which can be Analog if you want.

    the data logger can log all sensors on one card, you don`t need one for each image

    your reed is best on a Digital pin.

    you would write the value of each device to the card one at a time, and keep doing that at regular intervals, i think some people use a spreadsheet to look at the data afterwards.

    how they work is simply the same way that Memory works, like a digital camera stores pictures on an SD card, your SD card will store numbers instead of pictures for instance.

    as for shield (board) stacking, there isn`t really a limit exactly as long as it`s mechanically stable and and you don`t run out of power to run them, no need to solder them either, in fact I can`t imagine how you would solder them if you wanted to image

    I think that covers a few of your concerns for now, never apologise for questions either!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    it should relatively easily accomodate all those devices and maybe have a couple spare, assuming of course that your GPS is serial out.

    you have 19 pins, 6 of which can be Analog if you want.

    the data logger can log all sensors on one card, you don`t need one for each image

    your reed is best on a Digital pin.

    you would write the value of each device to the card one at a time, and keep doing that at regular intervals, i think some people use a spreadsheet to look at the data afterwards.

    how they work is simply the same way that Memory works, like a digital camera stores pictures on an SD card, your SD card will store numbers instead of pictures for instance.

    as for shield (board) stacking, there isn`t really a limit exactly as long as it`s mechanically stable and and you don`t run out of power to run them, no need to solder them either, in fact I can`t imagine how you would solder them if you wanted to image

    I think that covers a few of your concerns for now, never apologise for questions either!