Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Mega CNC. EasyDriver or Pololu Shield
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1297 views
  • Users 0 members are here
Related

Arduino Mega CNC. EasyDriver or Pololu Shield

eatumup
eatumup over 14 years ago

I'm sorry if this question has been answered to death but I still find myself a little confused. I have never built anything with stepper motors, especially a CNC machine.  I have been doing what reasearch I can and have so far determined that I should probably go with an Arduino Mega as the heart vs the Sanguinololu. It looks like theres plenty of code out there for the mega for this project. The thing that is confusing me is the stepper driver.

 

I have seen mostly the Pololu shield with thier 4 drivers used. But at $180 the Easy Driver looks tempting as I think the mega plus steppers come in at under 100.

 

So my question is, Can a CNC machine be done witht he mega and three EasyDrivers? Or is something missing without having the shield? Is one way reccomended over another? Would one have more limitations? Just looking for some advice on this one.

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 14 years ago

    It probably can.  The benefit of the shields and such is they usually do the voltage regulation on board, and have terminal blocks for the connections and limit switches, but I don't see why you cant just use the stepper boards directly.  Also, notice those steppers have low current, if you look at the pololu, they tend to support 1-2 amps.  If you want another one board solution, look at the Printrboard .  It's based on the teensy (which is an atmel chip with a usb bootloader) and I believe can run teensyduino code.

    http://printrbot.com/shop/printrboard-electronics/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eatumup
    0 eatumup over 14 years ago in reply to colecago

    Interesting. This helps a lot. One thing I overlooked was the amp rating of the Nema 17 motors that are typically used. The EasyDriver isn't rated for enough amperage. So this would cause a redesign. I will have to look into the Printrboard as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eatumup
    0 eatumup over 14 years ago in reply to colecago

    Interesting. This helps a lot. One thing I overlooked was the amp rating of the Nema 17 motors that are typically used. The EasyDriver isn't rated for enough amperage. So this would cause a redesign. I will have to look into the Printrboard as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Nate1616
    0 Nate1616 over 14 years ago in reply to eatumup

    I would look over at reprap.org.  they have some good documentation on stepper drivers and other methods for controling stepper motors.