Arduino
  • Products
  • More
Arduino
Arduino Forum Question about the 16-channel 12V module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 420 subscribers
  • Views 1853 views
  • Users 0 members are here
Related

Question about the 16-channel 12V module

e14 Contributor
e14 Contributor over 14 years ago

I have this module:http://www.sainsmart.com/16-channel-5v-relay-module-for-pic-arm-avr-dsp-arduino-msp430-ttl-logic.html

The 16-channel 12V module has a pair of 5v and GND pin among the low level inputs. Are those for reference voltage for the input pins or actually regulated 5v output voltage from the LM2576?

  • Sign in to reply
  • Cancel
Parents
  • dmaruska
    0 dmaruska over 14 years ago

    From what little I see on the schematic, You apply your own DC (12v) and the regulator will supply 5vdc to the on board control circuitry.  I can not see the header I/O, but it looks as if you will use a D I/O for each relay, but that is a guess with out more information on the circuit.  It also looks like there are some opto isolators to protect the controller device (Arduino, etc).  If there is a better schematic I can offer more information.  But that is a 12vdc to 5vdc regulator (Buck Switching).

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dmaruska
    0 dmaruska over 14 years ago

    From what little I see on the schematic, You apply your own DC (12v) and the regulator will supply 5vdc to the on board control circuitry.  I can not see the header I/O, but it looks as if you will use a D I/O for each relay, but that is a guess with out more information on the circuit.  It also looks like there are some opto isolators to protect the controller device (Arduino, etc).  If there is a better schematic I can offer more information.  But that is a 12vdc to 5vdc regulator (Buck Switching).

     

    Regards,

     

    Dave M.