Arduino
  • Products
  • More
Arduino
Arduino Forum Question about the 16-channel 12V module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 420 subscribers
  • Views 1848 views
  • Users 0 members are here
Related

Question about the 16-channel 12V module

e14 Contributor
e14 Contributor over 14 years ago

I have this module:http://www.sainsmart.com/16-channel-5v-relay-module-for-pic-arm-avr-dsp-arduino-msp430-ttl-logic.html

The 16-channel 12V module has a pair of 5v and GND pin among the low level inputs. Are those for reference voltage for the input pins or actually regulated 5v output voltage from the LM2576?

  • Sign in to reply
  • Cancel
Parents
  • R_Phoenix
    0 R_Phoenix over 14 years ago

    While sainsmart is a nice site and they have some cool stuff, V Lee is a spamer, posting his advertizements as a question.

     

    There is another too, Steve L I think it is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to R_Phoenix

    Believe it or not, I was not advertising. I do have question about it. And Sainsmart doesn't have the forum to discuss, (seems now they have built one), but not so popular, so I chose to post my question here. Sorry to make you feel that I am bothering others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to R_Phoenix

    Believe it or not, I was not advertising. I do have question about it. And Sainsmart doesn't have the forum to discuss, (seems now they have built one), but not so popular, so I chose to post my question here. Sorry to make you feel that I am bothering others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • R_Phoenix
    0 R_Phoenix over 14 years ago in reply to e14 Contributor

    Well my apologies, but why do you keep posting links to that site as questions, and then never reply to anyone trying to answer your questions? Usually only spamers do that.

     

    But to answer your questions, It will most likely take one digi pin per relay. Pin HIGH to close the relay (on) and LOW to open the realy (off). There is no mention that the relays are "addressable" indicating that they are RS-232RS-232 serial control, which would only be 2 wires for all 16. Also the schematic don't quit look right to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to R_Phoenix

    I am new to forum and I don't realize the rules. I am just seeking some answers. I didn't realize the reply, the reminding emails went to spam box. Thank you all for your reply. It does help a lot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 14 years ago in reply to e14 Contributor

    It looks like the same sort of board is offered by quite a few vendors, and this listing has more information about the way things are hooked up:

    http://www.ebay.ca/itm/16-Channel-12V-Relay-Module-Arduino-PIC-ARM-DSP-AVR-/230642906093?pt=LH_DefaultDomain_0&hash=item35b36373ed#ht_3327wt_1170

     

    By the look of their schematics, you will need one Arduino pin per relay. From what I can tell, you have to also provide it with 5 volts and ground from the Arduino as well, and you have to do that twice because there are two chips that take the 5 volt signals to the 12 volt level. (JP2)

    And it looks like you have to separately provide it 12 volts and ground as well.

     

    Anyhow, that's my best guess based on those diagrams. I suppose you could start by hooking up the 12v and its corresponding gnd, and then check if the JP2 pins are giving you 5volts, just to make sure.

     

    Out of curiosity, what are building that needs 16 relays?