Arduino
  • Products
  • More
Arduino
Arduino Forum I need help please .....it's important for my graduation project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 230 views
  • Users 0 members are here
Related

I need help please .....it's important for my graduation project

e14 Contributor
e14 Contributor over 14 years ago

Hi ,i need some help please....I want to know how to take temperature reading from LM75 temperature sensor and store it ,then it will be taken by wireless node"zig bee"  and i use arduino uno........please i need answer quickly  ,thank you for your time

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 14 years ago

    Cool project.  Which parts do you have working so far?  I would think that the LM75 data sheet should be of great help to you.  Also you need to search at arduino.cc. 

    I could not locate any LM75 info at tronixstuff.wordpress.com.  It is a great place to get up to speed with arduino uno.

     

    REF: lm75a.pdf

    "I2C-bus serial interface

    The LM75A can be connected to a compatible 2-wire serial interface I2C-bus as a slave

    device under the control of a controller or master device, using two device terminals, SCL

    and SDA. The controller must provide the SCL clock signal and write/read data to/from the

    device through the SDA terminal. Notice that if the I2C-bus common pull-up resistors have

    not been installed as required for I2C-bus, then an external pull-up resistor, about 10 kW,

    is needed for each of these two terminals. The bus communication protocols are

    described in Section 7.10."

     

    For a more user friendly presentation please see http://tronixstuff.wordpress.com/2010/10/20/tutorial-arduino-and-the-i2c-bus/.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 14 years ago

    Cool project.  Which parts do you have working so far?  I would think that the LM75 data sheet should be of great help to you.  Also you need to search at arduino.cc. 

    I could not locate any LM75 info at tronixstuff.wordpress.com.  It is a great place to get up to speed with arduino uno.

     

    REF: lm75a.pdf

    "I2C-bus serial interface

    The LM75A can be connected to a compatible 2-wire serial interface I2C-bus as a slave

    device under the control of a controller or master device, using two device terminals, SCL

    and SDA. The controller must provide the SCL clock signal and write/read data to/from the

    device through the SDA terminal. Notice that if the I2C-bus common pull-up resistors have

    not been installed as required for I2C-bus, then an external pull-up resistor, about 10 kW,

    is needed for each of these two terminals. The bus communication protocols are

    described in Section 7.10."

     

    For a more user friendly presentation please see http://tronixstuff.wordpress.com/2010/10/20/tutorial-arduino-and-the-i2c-bus/.