Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino crane machine
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 416 subscribers
  • Views 1189 views
  • Users 0 members are here
Related

Arduino crane machine

e14 Contributor
e14 Contributor over 14 years ago

im thinking about using the arduino mega w/ ramps sheild to power a crane assembly from an old machine i would like help with this since this is my first arduino project

  • Sign in to reply
  • Cancel
Parents
  • billabott
    0 billabott over 14 years ago

    Great!  How big is your crane?

     

    I am reading Dustyn Robert's "Making Things Move DIY Mechanisms for Inventors, Hobbyists, and Artists".  I highly recommend it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to billabott

    box that the motors are in are 22 In. by 6 1/4 in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 14 years ago in reply to e14 Contributor

    These are stepper motors, yes?  What are the motors rated?  voltage and amps max under load.

    The Kysan  1124090 Nema 17 motors recommended by Ultimachine for that control board have the following specifications:

    • Model number:  1124090
    • Holding Torque:  5.5Kg.cm
    • Rated Voltage:  4.2V
    • NO.of Phase:  2
    • Step Angle:  1.8° ± 5%
    • Resistance Per Phase:  2.8Ω± 10%
    • Inductance Per Phase:  4.8mH± 20%
    • Current Per Phase:  1.5A
    • Shaft:  5mm diameter w/ one flat
    • Insulation Class:  Class B
    • Dielectric Strength:  100Mohm
    • Operation Temp Range:  -20 ~ +40° C
    • Lead Wire:  22AWG / 750mm
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • billabott
    0 billabott over 14 years ago in reply to e14 Contributor

    These are stepper motors, yes?  What are the motors rated?  voltage and amps max under load.

    The Kysan  1124090 Nema 17 motors recommended by Ultimachine for that control board have the following specifications:

    • Model number:  1124090
    • Holding Torque:  5.5Kg.cm
    • Rated Voltage:  4.2V
    • NO.of Phase:  2
    • Step Angle:  1.8° ± 5%
    • Resistance Per Phase:  2.8Ω± 10%
    • Inductance Per Phase:  4.8mH± 20%
    • Current Per Phase:  1.5A
    • Shaft:  5mm diameter w/ one flat
    • Insulation Class:  Class B
    • Dielectric Strength:  100Mohm
    • Operation Temp Range:  -20 ~ +40° C
    • Lead Wire:  22AWG / 750mm
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer