Arduino
  • Products
  • More
Arduino
Arduino Forum CNC Software. What to use?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 420 subscribers
  • Views 2971 views
  • Users 0 members are here
Related

CNC Software. What to use?

eatumup
eatumup over 14 years ago

I have started my project to build a CNC router using an Auduino Mega 2560, Ramps 1.4 and A4988 stepper drivers. While working on building the hardware I am struggling sorting out the various pieces of software I need. The goal  is to do everything open source in windows preferably but not oppsed to using linux.  What I am looking for is a clear guide to what I will need to create the element, upload the gcode and what software I need to upload to the mega. I was hoping that someone here could confirm or correct my understanding of how this would go.

 

Looking at reprap.org I would:

 

1) Create an STL file using something such as OpenSCAD or FreeCAD (any reccomendations on cad programs?)

2) Open the STL file in something like RepSnapper or RepRap Host Software to generate the g-code.

3) Exicute the build order from Rep software.

Is this correct?

 

Some of the elemetns that I am worried about /havent quite figured out is the sofware for the Arduino and the fact that all these instructions are based on adding material rather than subtracting.

 

Do I just upload the Reprap firmware and go? Do I need to use different firmware or gcode generating software? Or do I need both different g-code generating software and firmware for milling? Any help sorting this out would be most appreciative.

  • Sign in to reply
  • Cancel

Top Replies

  • eatumup
    eatumup over 14 years ago in reply to ntewinkel +1
    Nico, Got an answer from another forum on this. What G-code interpreter/uploader I should use? or does it really matter? The G-code interpreter is the same if it is removing material or adding it. What…
  • e14 Contributor
    e14 Contributor over 14 years ago +1 suggested
    I think that there are several pieces of software around that suit people with deep pockets, but if you want to drive a CNC machine and your pockets are almost empty after buying and making everything…
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I think that there are several pieces of software around that suit people with deep pockets, but if you want to drive a CNC machine and your pockets are almost empty after buying and making everything else, you should look at EMC2, which is open source and therefore free.....Some people swear by it and some at it. The manual is quite thick and very extensive......but so are the manuals for other softwares that you must buy......

     

    Its Linux, but you can install ubuntu in a seperate partition on the same disk as Windows if you wish. Read more here:- http://www.linuxcnc.org/

     

    It appears to be very complete, but as with any software, there is a lot to learn and it can be heavy going I am told......

     

    Maybe there are some others here that can add further infos....

     

    regards

     

    Andy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • eatumup
    0 eatumup over 14 years ago in reply to e14 Contributor

    oops nevermind. I was going to ask for a link to EMC2 thinking that linuxcnc is different. Looks like linuxcnc is just the websire for emc2. Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • eatumup
    0 eatumup over 14 years ago in reply to e14 Contributor

    oops nevermind. I was going to ask for a link to EMC2 thinking that linuxcnc is different. Looks like linuxcnc is just the websire for emc2. Thanks