Arduino
  • Products
  • More
Arduino
Arduino Forum Make LEDs blink in rhythm with music code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 4 answers
  • Subscribers 419 subscribers
  • Views 2749 views
  • Users 0 members are here
Related

Make LEDs blink in rhythm with music code

e14 Contributor
e14 Contributor over 14 years ago

Hello fellow Arduino users,

 

I have a code that plays the Popcorn song, feel free to use it or change it for yourself:

 

#include "pitches.h"

//The Pin for 8ohm speaker is 8....

int melody[] = {

  NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_DS5, NOTE_G5, NOTE_C5, 0,

  NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_DS5, NOTE_G5, NOTE_C5, 0,

  NOTE_C6, NOTE_D6, NOTE_DS6, NOTE_D6, NOTE_DS6, NOTE_C6, NOTE_D6, NOTE_C6,

  NOTE_D6, NOTE_AS5, NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_C6, 0,

  NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_DS5, NOTE_G5, NOTE_C5, 0,

  NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_DS5, NOTE_G5, NOTE_C5, 0,

  NOTE_C6, NOTE_D6, NOTE_DS6, NOTE_D6, NOTE_DS6, NOTE_C6, NOTE_D6, NOTE_C6,

  NOTE_D6, NOTE_AS5, NOTE_C6, NOTE_AS5, NOTE_C6, NOTE_G5, NOTE_C6,

};

 

// note durations: 4 = quarter note, 8 = eighth note, etc.:

int noteDurations[] = {

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4,4,4,

  4,4,4,4,4,4

  };

void setup() {

  for (int thisNote = 0; thisNote < 64; thisNote++) {

    int noteDuration = 900/noteDurations[thisNote];

    tone(8, melody[thisNote],noteDuration);

    int pauseBetweenNotes = noteDuration * 1;

    delay(pauseBetweenNotes);

    noTone(8);

  }

 

}

void loop() {

}

 

I want to make the LEDs blink in rhythm with the beeps of my tiny Arduino "player"

 

I have an Arduino Mega 2560 R3

 

What can I add to my code to make one or more LEDs blink in rhythm with the music?

  • Sign in to reply
  • Cancel

Top Replies

  • windsr
    windsr over 14 years ago in reply to e14 Contributor +1
    I like your idea too. I haven't done any programming for about 20yrs so I'm learning again, these little projects are a great place to learn. Thanks for sharing.
  • billabott
    billabott over 14 years ago in reply to ntewinkel +1
    Hi Nico. With regards to the stripboard layout method shown in the digikey project referenced above. What would you recommend for a smaller size board of 20 x 46 hole pattern They say to "Mark the top…
Parents
  • donnacarter0103
    0 donnacarter0103 over 8 years ago

    See this: https://forum.processing.org/two/discussion/3474/need-help-getting-leds-to-flash-to-music

    It gives you the solution for blinking LEDs in rhythm.

    I have also make a blog on making LEDs Flash to music using Arduino UNO board. If you need more information visit my article.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • donnacarter0103
    0 donnacarter0103 over 8 years ago

    See this: https://forum.processing.org/two/discussion/3474/need-help-getting-leds-to-flash-to-music

    It gives you the solution for blinking LEDs in rhythm.

    I have also make a blog on making LEDs Flash to music using Arduino UNO board. If you need more information visit my article.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer